cancel
Showing results for 
Search instead for 
Did you mean: 

"STM32G474_MB1303_DRP_ONLY" build break at "USBPD_PE_Request_CtrlMessage"

qqGHUAN
Associate II

I have tried the application "STM32G474_MB1303_DRP_ONLY" from STUSB014-v1.1.1 to start my development. but there is a build break by some function in usbpd_core.h.

But the related files and libraries are included in my project and listed in the project explorer.

is there any step need to check??

using CubeIDE 1.9

Thanks a lot

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Mike_ST
ST Employee

Hello,

Same here...

For some reason the library USBPDCORE_PD3_CONFIG_MINDRP_CM4_wc32 is not linked, as specified in the project settings.

As a temporary fix, please check my attached picture

View solution in original post

2 REPLIES 2
Mike_ST
ST Employee

Hello,

Same here...

For some reason the library USBPDCORE_PD3_CONFIG_MINDRP_CM4_wc32 is not linked, as specified in the project settings.

As a temporary fix, please check my attached picture

Hi Mike_ST

Thanks for your answer

it works!!​