2026-05-18 10:12 PM
I would like to use the board's built-in microphone to display audio data visualization on an LCD screen. I want to add more display modes later, but at the moment I only have basic waveform time domain display.
I use the built-in microphone to record audio, which I then convert to PCM using PDM2PCM middleware. However, there seem to be no correlation between the sound and the pcm values. Whether I speak, turn the music on, or do nothing at all - pcm values are about the same.
Moreover, every position in the PCM buffer hovers around the same value. For example, some positions are about ~-11000 no matter what, and the other are about ~20k no matter what. So, the audio visualization is almost flat with some random noise.
I assume that there is something wrong with how I use the mic or pdm2pcm.
The I2S and middleware settings
Example PCM values
The code
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void MX_FREERTOS_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
//base color and line color
uint16_t BASE_COLOR = YELLOW;
uint16_t DISPLAY_COLOR = BLUE;
//TASK HANDLES
//a task to send output to the screen
TaskHandle_t xScreenTaskHandle = NULL;
//a task to communicate with the phone via bluetooth
TaskHandle_t xBTTaskHandle = NULL;
//a task to read sensor outputs
TaskHandle_t xDataProcessHandle = NULL;
//PDM T PCMS
extern PDM_Filter_Handler_t PDM1_filter_handler;
//SAMPLE BUFFER
#define MIC_PDM_BUFFER_TOTAL 256
#define MIC_PCM_BUFFER_TOTAL 512 //MIC_BUFFER_TOTAL / 16
volatile uint16_t pdmBuffer[MIC_PDM_BUFFER_TOTAL];
volatile int16_t pcmBuffer[MIC_PCM_BUFFER_TOTAL];
uint32_t pcmBufferNext = 0; //where to write samples next
//current mode of display (https://huggingface.co/learn/audio-course/chapter1/audio_data)
//https://source-separation.github.io/tutorial/basics/representations.html
enum display_mode_enum {SPECTOGRAM, //same as frequency bars but with range
WAVEFORM, //sound as waveform
FREQUENCY_BARS, //split audio into frequence ranges and show the energy in each range as a bar
OCTAVE_BANDS, //musical octaves rather than frequency bars
STOP};
volatile enum display_mode_enum display_mode = WAVEFORM;
//waveform settings and values
volatile uint32_t waveWaitSamples = 512; //48000/1000 = 48Hz
volatile uint32_t waveAmp = 70;
volatile int16_t minSample = INT16_MAX;
volatile int16_t maxSample = INT16_MIN;
volatile uint32_t sampleCount = 0;
volatile uint16_t screenPtr = 0;
volatile uint16_t dmaBufCol[ILI_SCREEN_HEIGHT];
//bluetooth variables
#define UART_BUFFER_SIZE 1
uint8_t UART2_rxBuffer[UART_BUFFER_SIZE];
//INTERRUPT HANDLERS
//SPI DMA interrupt
void HAL_SPI_TxCpltCallback(SPI_HandleTypeDef *hspi) {
if (hspi->Instance == ILI_SPI_HANDLE.Instance) {
ILI_DMA_Callback();
}
}
//I2S DMA interrupt
void HAL_I2S_RxCpltCallback(I2S_HandleTypeDef *hi2s) {
printf("full i2s\n");
BaseType_t xHigherPriorityTaskWoken = pdFALSE;
/* Cast pointer to uint32_t and send as notification value */
xTaskNotifyFromISR(xDataProcessHandle,
(uint32_t)&pdmBuffer[MIC_PDM_BUFFER_TOTAL/2], /* first half pointer */
eSetValueWithOverwrite,
&xHigherPriorityTaskWoken);
portYIELD_FROM_ISR(xHigherPriorityTaskWoken);
}
void HAL_I2S_RxHalfCpltCallback(I2S_HandleTypeDef *hi2s) {
printf("half i2s\n");
BaseType_t xHigherPriorityTaskWoken = pdFALSE;
/* Cast pointer to uint32_t and send as notification value */
xTaskNotifyFromISR(xDataProcessHandle,
(uint32_t)&pdmBuffer[0], /* first half pointer */
eSetValueWithOverwrite,
&xHigherPriorityTaskWoken);
portYIELD_FROM_ISR(xHigherPriorityTaskWoken);
}
//task functions
void dataProcessTask(void * pvParameters ) {
uint32_t ulNotifiedValue;
while(1) {
//wait for the data
xTaskNotifyWait(0, 0xFFFFFFFF, &ulNotifiedValue, portMAX_DELAY);
//process the data
printf("data received, the address of the array is %d \n", ulNotifiedValue);
//convert pdm to pcm for further analysis and buffer it
//uint16_t pcmBuff[32];
PDM_Filter((uint8_t *)ulNotifiedValue, &pcmBuffer[pcmBufferNext], &PDM1_filter_handler);
//reset min/max
//iterate over all newly received samples
for (int i = 0; i < 32; i++) {
if (pcmBuffer[pcmBufferNext + i] < minSample) {
minSample = pcmBuffer[pcmBufferNext + i];
} else if (pcmBuffer[pcmBufferNext + i] > maxSample) {
maxSample = pcmBuffer[pcmBufferNext + i];
}
}
//update PCM buffer index
pcmBufferNext = (pcmBufferNext + 32) % MIC_PCM_BUFFER_TOTAL;
//now, find min/max values for the buffer
sampleCount += 32;
if (sampleCount == waveWaitSamples) {
sampleCount = 0; //update the sample count
//wake up the screen task
xTaskNotify(xScreenTaskHandle, 0, eSetValueWithOverwrite);
minSample = INT16_MAX; // reset HERE, not in screenTask
maxSample = INT16_MIN;
}
}
}
//convert from -32,768 to 32,767 range to 0-320 range
uint16_t pcmToLCD(int16_t pcm, uint32_t waveAmp) {
uint32_t usable = 240 * waveAmp / 100;
uint32_t offset = (240 - usable) / 2;
return (uint16_t)(((int32_t)pcm + 32768) * usable / 65535 + offset);
}
//shift the screen leftwards
void shiftLeft() {
screenPtr = (screenPtr + 1) % 320; //update the VSP
ILI_Write_Command(0x37);
ILI_Write_Data((uint8_t)((screenPtr >> 8) & 0xFF)); //first half of VSP
ILI_Write_Data((uint8_t)((screenPtr) & 0xFF)); //second half of VSP
}
void drawWave(uint16_t minLCD, uint16_t maxLCD) {
//first, shift the screen buffer
shiftLeft();
//clear and draw the column
uint16_t colAddr = (screenPtr + 319) % 320;
for (int i = 0; i < ILI_SCREEN_HEIGHT; i++) {
if ((i >= minLCD) && (i <= maxLCD)) {
dmaBufCol[i] = DISPLAY_COLOR;
} else {
dmaBufCol[i] = BASE_COLOR;
}
}
ILI_Set_Address(colAddr, 0, 1, 240); //clear the whole column
ILI_DMA_Load(dmaBufCol);
//ILI_DMA_Fill(BASE_COLOR);
//display the column
//ILI_Set_Address(colAddr, minLCD, 1, maxLCD - minLCD); //rewrite the column
//ILI_DMA_Fill(DISPLAY_COLOR);
}
void screenTask(void * pvParameters ) {
uint32_t ulNotifiedValue;
while(1) {
//https://huggingface.co/learn/audio-course/chapter1/audio_data
//wait for the data
xTaskNotifyWait(0, 0xFFFFFFFF, &ulNotifiedValue, portMAX_DELAY);
//process the data
switch (display_mode) {
case SPECTOGRAM:
break;
case WAVEFORM:
uint16_t minLCD = pcmToLCD(minSample, waveAmp);
uint16_t maxLCD = pcmToLCD(maxSample, waveAmp);
drawWave(minLCD, maxLCD);
break;
case FREQUENCY_BARS:
break;
case OCTAVE_BANDS:
break;
case STOP:
break;
default:
}
printf("data displayed\n");
}
}
void btTask(void *pvParameters) {
while(1) {
}
}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_I2S2_Init();
MX_SPI3_Init();
MX_USART1_UART_Init();
MX_CRC_Init();
MX_PDM2PCM_Init();
/* USER CODE BEGIN 2 */
//turn on the screen
HAL_GPIO_WritePin(Screen_BL_GPIO_Port, Screen_BL_Pin, GPIO_PIN_SET);
//init screen
ILI_Init();
//set rotation
//ILI_Set_Rotation(SCREEN_HORIZONTAL_2);
//fill it with the default color
ILI_DMA_Fill(BASE_COLOR);
//test
//clear and draw the column
//while(ILI_DMA_Busy());
//uint16_t colAddr = (screenPtr + 319) % 320;
//uint16_t dmaBuf[ILI_SCREEN_HEIGHT];
//for (int i = 0; i < ILI_SCREEN_HEIGHT; i++) {
//if ((i >= 10) && (i <= 200)) {
//dmaBuf[i] = DISPLAY_COLOR;
//} else {
// dmaBuf[i] = BASE_COLOR;
//}
//}
//ILI_Set_Address(10, 0, 1, 240); //clear the whole column
//ILI_DMA_Load(dmaBuf);
//create tasks
//first DMA transfer (uncomment later)
HAL_I2S_Receive_DMA(&hi2s2, pdmBuffer, MIC_PDM_BUFFER_TOTAL);
//bluetooth listen
HAL_UART_Receive_IT(&huart1, UART2_rxBuffer, UART_BUFFER_SIZE);
//tasks
BaseType_t xReturned;
/* Create the task, storing the handle. */
xReturned = xTaskCreate(
dataProcessTask, /* Function that implements the task. */
"data_proc_task", /* Text name for the task. */
2048, /* Stack size in words, not bytes. */
( void * ) NULL, /* Parameter passed into the task. */
2,/* Priority at which the task is created. */
&xDataProcessHandle); /* Used to pass out the created task's handle. */
xReturned = xTaskCreate(
screenTask, /* Function that implements the task. */
"screen_update_task", /* Text name for the task. */
1024, /* Stack size in words, not bytes. */
( void * ) NULL, /* Parameter passed into the task. */
3,/* Priority at which the task is created. */
&xScreenTaskHandle); /* Used to pass out the created task's handle. */
xReturned = xTaskCreate(btTask,
"blt_task",
512,
(void*)NULL,
1,
&xBTTaskHandle);
vTaskStartScheduler();
/* We should never get here as control is now taken by the scheduler */
/* USER CODE END 2 */
/* We should never get here as control is now taken by the scheduler */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
2026-05-18 10:23 PM
I'm pretty sure the "legacy" SPL-based F407 discovery firmware contains an example project for the microphone, if I remember correctly the demo application it came with.
> I would like to use the board's built-in microphone to display audio data visualization on an LCD screen.
And the SPL firmware contained decent drivers for the STM32F4DIS-LCD module, which I used in quite a few projects.
The F407 discovery was released quite a while before Cube/HAL, so the demo and driver support might be lacking. To be honest, all my F407 discovery projects are based upon SPL code.
2026-05-18 10:43 PM
Where can I have a look at the SPL example project for the microphone?
2026-05-18 11:57 PM
Still available from ST : https://www.st.com/en/embedded-software/stsw-stm32068.html
2026-05-19 1:19 AM
Hello,
Use the board's BSP driver or use it as reference:
2026-05-19 1:35 AM - edited 2026-05-19 1:36 AM
My experience is, that one good way how to observe audio is... to listen to it.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.