2019-08-01 8:25 AM
Hi,
I have custom board for stmf401 and I try to program it in DFU mode. I set the boot0 to 1 and reset the chip but it is not recognized as DFU device. (not listed in the DfuSe).
Do I miss any procedure or settings?
(I have connected the PA11/PA12 pins to the corresponding pins in USB).
Thanks in advance.
Duncan
Solved! Go to Solution.
2019-08-01 8:57 AM
App Note AN2606 should provide indications if it is supported.
You'd need an external HSE oscillator, that would need to start, and be at a frequency blessed by the firmware, some STM32 had specific expectations, some not, again check AN2606 for specifics.
2019-08-01 8:57 AM
App Note AN2606 should provide indications if it is supported.
You'd need an external HSE oscillator, that would need to start, and be at a frequency blessed by the firmware, some STM32 had specific expectations, some not, again check AN2606 for specifics.
2019-08-02 7:44 AM
Yes, I checked the note and it is supported and It did miss the external HSE oscillator for it.
Thank you very much.