2018-11-21 12:32 AM
I want to signal a possible bug in CubeMx version 4.27, in the STM32L4xx HAL library package. In the ADC configuration of the external trigger, the TIM4 TRGO setting does not work.
I think the error is in line 518 of file "stm32l4xx_hal_adc.h". The original is:
#define ADC_EXTERNALTRIG_T4_TRGO (LL_ADC_REG_TRIG_EXT_TIM4_CH4)
but it should be:
#define ADC_EXTERNALTRIG_T4_TRGO (LL_ADC_REG_TRIG_EXT_TIM4_TRGO)
2018-11-22 08:46 AM
Hello @GZini.16 ,
Please note that this typo is reported to our development team to implement the fix in stm32l4xx_hal_adc.h.
Thanks for reporting it.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.