2021-07-04 4:44 AM
There are eSIM and Mirco_SIM in the Modem board, but it keep report:
CST_modem_sim_init : Can't find sim on current slot. Increment sim slot.
CST_modem_sim_init : No more sim slot, no SIM found. Retry...
Any suggestion?
2021-07-05 3:21 AM
Dear @New.Fish
I understand that you have inserted a SIM card in the micros SIM slot of the Modem Board. Can you share the trace from the terminal so that we can make more detail analysis of the issue?
Thanks a lot
Best Regards
Solofo
2021-07-05 5:58 AM
2021-07-05 11:42 AM
Hello,
Can you confirm if you have inserted a SIM card in the micoro SIM socket slot?
If this is the case, then I suggest to update first the Modem FW to be compatible with X-CUBE-CELLULAR.
The instruction to update the Modem Firmware is provided in the
\STM32CubeExpansion_CELLULAR_V6.0.0\Utilities\Modem_FW\BG96\
Let me know if you still have issue.
Best Regards
Solofo
2021-07-11 8:47 PM
Hello,
I try to use "QFlash" to update the Cellular firmware, the "QFlash" get problem with Win7 and Win 10 PC, I contact Quectel FAE this stage.
Reagrsd
2021-07-12 2:52 AM
By default, this demo software is connected to eSIM or MicroSIM?
It suppose have 3 months of free usage, I follow the instruction, but I can't make it work, what's wrong?
2021-07-17 2:54 AM
Hello,
Quectel FAE send me the latest Cellular firmware, and the DVK can find the MicroSIM now.
I believe the file in \STM32CubeExpansion_CELLULAR_V6.0.0\Utilities\Modem_FW\BG96\ is obsoleted.
I'm still interested in the eSIM, this is a feature for the product which our customer don't need buy SIM card.
Question: How can I make the eSIM work? I can't find the datasheet for this eSIM.