cancel
Showing results for 
Search instead for 
Did you mean: 

OTA not able to powerup new firmware image

saraiahd
Associate II

Hi,

I am trying to perform OTA on STM32F413ZT6 using Seirra Wi-Fi module. 

The Sierra and MCU communicate over UART. Here the binary is downloaded by the WI-Fi from a server, further, it will send the binary to the MCU. The STM is responsible for writing it to the application partition using a custom bootloader and booting up the newly written binary.

From the above-mentioned process, I am able to perform all the initial steps of downloading the file, transferring it over UART and writing it to flash. But when it comes to booting the new application, it's not working for me. I have also configured the vector table and application address correctly for the application.

0 REPLIES 0