cancel
Showing results for 
Search instead for 
Did you mean: 

OTA implementation stm32l072

satyam9896
Associate II

SO I HAVE STARTED MY PROJECT WITH STM32L072 SERIES WHICH IS HAVING 192B FLASH 64 PIN IC along with bluenrg-m2sa. my concern and doubt is regarding implementation of ota feature to stm32l072 ic which i never implemented and work on before and also the examples and other refrences are mostly availabe for L4 or F series IC so my request to give me and help me with appropriate resoures and file so that i can easily implement the ota feature to my project and can easily understand also.

21 REPLIES 21

AN2606 define system loader supported interfaces, you read ??? 

Ya i red that and understood about booting and all however im working on ble advertisement and ota feature enabling in sensor mobile app ones its done i will be using one fn too recieve the data(firmware image and save it at perticular addresss with the help of flash write fn). i need to know about those characterstics and services and than how to varify it)