User Activity

Hi Everyone,I am working on enabling Direct Test Mode (DTM) for BLE-SPBTLE-RF, which is connected to my STM32L053 via SPI1 on a custom PCB. The goal is to perform RF testing so I can submit the board for regulatory certification.Hardware Setup:MCU: S...
Hello ST Community,I am working on an OTA (Over-The-Air) update implementation for an STM32L072 series microcontroller which has 192kb flash memory. In my setup, I have divided the flash memory into three regions: bootloader (starting at 0x08000000),...
Split from this thread: https://community.st.com/t5/stm32-mcus-embedded-software/flash-writing/td-p/753438 Hi @mƎALLEm  thanks and   void StartUpdateFWBlueNRG(uint32_t SizeOfUpdate, uint32_t uwCRCValue) { __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_PGAERR); ...
Hi All, trying to write data into flash with dynamical flash address selection approach but it fails but at same time if hash(#) define the address the flash programming all works fine, Please suggest me the best solution and explain me the issues ch...
SO I HAVE STARTED MY PROJECT WITH STM32L072 SERIES WHICH IS HAVING 192B FLASH 64 PIN IC along with bluenrg-m2sa. my concern and doubt is regarding implementation of ota feature to stm32l072 ic which i never implemented and work on before and also the...