2025-01-30 1:16 AM
Hello Forum,
I would appreciate some advice regarding bootloaders. Apologies in advance as this is mostly new to me. I have been researching the pre-programmed ST System Bootloader and OpenBootLoader (OBL) to try and figure out whether they are appropriate for firmware update in our product. Our product will most likely contain multiple STM32U5 MCUs connected together on a CAN bus. Firmware update will be performed from a Windows PC either connected to the same CAN bus or via USB to the 'main' MCU. The main 'MCU' is likely to have a 64MB filesystem available to it.
Assuming we decide to use the ST SystemBootloader then these questions come to mind:
Assuming we decide to use the OpenBootloader at the start of flash and the application at an offset from that like this:
----------------------
(ROM)
SystemBootloader --|
---------------------- <-| Jump (option byte settings)
(Flash)
OpenBootLoader --| On Go Command
---------------------- <-| Jump
(Flash)
Application
----------------------
The SystemBootloader loads runs OpenBootloader. This, so far as I can tell by looking at the code, will sit forever waiting for the GO command which is not want we want if an application has already been programmed. How should we approach this? It seems to me that there needs to be a mechanism to tell OpenBootLoader to just jump to the application but I'm 0% sure of this as I have no experience. What would be the right way?
Any advice much appreciated.
/P
2025-01-31 7:16 AM
Hello @DenzilDexter
Please refer to this article to implement your boot process.
2025-01-31 7:25 AM - edited 2025-01-31 7:38 AM
I ve been down this road already a couple of times.
>>Our product will most likely contain multiple STM32U5 MCUs connected together on a CAN bus.
https://community.st.com/t5/stm32-mcus-products/is-the-stm-system-bootloader-trough-canbus-just-not-woking-when/m-p/165204
System bootloader (Trough classic CAN or FDCAN) doesnt like multi node canbus buses so not suitable for your application unless you do some trick disabling the canbus of every non-being-updated node.
Go straight to develop your own CAN bootloader (maybe based on openBL so you can use CUBEprogrammer and stlink)
>> I cannot see a way to verify the image on the target.
Cube Programmer verifies (by reading back) after writting to flash, see my cubeprogrammer logs from today using my own openBL based bootloader
15:16:19 : STM32CubeProgrammer API v2.18.0 | Windows-64Bits
15:16:27 : UR connection mode is defined with the HWrst reset mode
15:16:27 : ST-LINK FW : V3J8M1B5
15:16:27 : Voltage : 0.00V
15:16:27 : Bridge Freq : 48000 KHz
15:16:27 : Baudrate : 125 Kbps
15:16:27 : BL version : 2.0
15:16:27 : Device ID : 0x469
15:16:28 : UPLOADING OPTION BYTES DATA ...
15:16:28 : Bank : 0x00
15:16:28 : Address : 0x1fff7800
15:16:28 : Size : 36 Bytes
15:16:28 : Bank : 0x01
15:16:28 : Address : 0x1ffff808
15:16:28 : Size : 36 Bytes
15:16:28 : Bank : 0x02
15:16:28 : Address : 0x1fff7828
15:16:28 : Size : 4 Bytes
15:16:28 : Bank : 0x03
15:16:28 : Address : 0x1ffff828
15:16:28 : Size : 8 Bytes
15:16:28 : UPLOADING ...
15:16:28 : Size : 1024 Bytes
15:16:28 : Address : 0x8000000
15:16:28 : Read progress:
15:16:28 : Data read successfully
15:16:28 : Time elapsed during the read operation is: 00:00:00.208
15:16:49 : Opening and parsing file: nucleog474_blinky.elf
15:16:49 : Memory Programming ...
15:16:49 : File : nucleog474_blinky.elf
15:16:49 : Size : 5.80 KB
15:16:49 : Address : 0x08008000
15:16:49 : Erasing memory corresponding to segment 0:
15:16:49 : Erasing internal memory sectors [16 18]
15:16:49 : Download in Progress:
15:17:06 : File download complete
15:17:06 : Time elapsed during download operation: 00:00:17.085
15:17:06 : Verifying ...
15:17:06 : Read progress:
15:17:08 : Download verified successfully
15:17:08 : RUNNING Program ...
15:17:08 : Address: : 0x08008000
15:17:08 : Start operation achieved successfully
>> I see the SystemBootloader can only cope with 1 CAN node
Exactly, some people use UART and start shapped conections
>>This, so far as I can tell by looking at the code, will sit forever waiting for the GO command which is not want we want if an application has already been programmed. How should we approach this?
You could implement a software timeout or configure the IWDG (openbootloader already did half of the work there)
To stay 1s or 2s waiting for bootloading commands and after that jumping to your APP (if memory is not empty and checksum is alright )
2025-02-04 12:13 AM
Thanks Saket, I had seen that.
2025-02-04 12:25 AM
Javier, thanks for taking the time to reply in such detail. I think we will go down the route of modifying OpenBootLoader to meet our needs. Our current thinking is that the bootloader (BL) will jump to the application if one has been programmed (magic # in flash at some predefined address) - otherwise it will sit waiting to be asked to do something. We will incorporate into the application the means to jump to the BL on command.
Our main MCU will control the firmware update of the other MCUs in the system over CAN using a mechanism of our own making. I have CANopen working on an STM32 F303K8TX and so maybe we'll use the SDO protocol in it - otherwise we'll just transmit CAN frames.
On the subject of image validation I was thinking more about whether the image supplied by the PC is one that should be programmed onto the devices - so rather than a simple CRC I had envisaged a digital signature. This would be validated before programming even began. Any thoughts on this would be welcome.