cancel
Showing results for 
Search instead for 
Did you mean: 

only interrupt once for HAL_SPI_RxCpltCallback

Jiannong Zhou
Associate II

Configured Master/Slave SPI.

(1). trigger Interrupt SPI receive.

(2). Interrupt and receive a data

(3). Trigger interrupt SPI receive again

(4). Never trigger SPI Interrupt receive.

...

HAL_SPI_Receive_IT(&hspi1, SPI_Receive_Buffer, SPI_RECEIVE_DATA_LENGTH);

 while (1)

 {

if(SPI_Frame_Reveived)

{

SPI_Frame_Reveived = 0;

HAL_SPI_Receive_IT(&hspi1, SPI_Receive_Buffer, SPI_RECEIVE_DATA_LENGTH);

}

 }

...

Interrupt:

void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)

{

SPI_Frame_Reveived = 1;

}

Why SPI receive IT only once?

Jiannong

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Bob S
Super User

Did you step through your code in main() and see what happens (or doesn't happen) to SPI_Frame_Received?

How and where do you declare SPI_Frame_Received? I'm guessing something like "int SPI_Frame_Received". It needs to be declared as "volatile", otherwise the code in main() will never see the change made in the callback.

Jiannong Zhou
Associate II

Hi Bob S,

thanks for your suggestion.

For SPI_Frame_Reveived, I declared in main()

uint8_t SPI_Frame_Reveived

I will try to declare as "volatile".

And I tried to add the code below in main() loop. it seems that it can be interrrupted.

HAL_SPI_Receive_IT(&hspi1, SPI_Receive_Buffer, SPI_RECEIVE_DATA_LENGTH);

/* Receive command from Master */

while (HAL_SPI_GetState(&hspi1) != HAL_SPI_STATE_READY) {}

I do not know why we keep running "HAL_SPI_Receive_IT".

Jiannong