2025-05-26 10:24 AM
Hi there,
I have found an issue in code generation where there is a mismatch between a variable declaration in tsl_user.h and its definition in tsl_user.c.
The bug can be reproduced by following these steps:
Create a new project using the board selector tab and select "NUCLEO-L152RE".
Enable TS and TOUCHSENSING in the .ioc
In TS, allocate 8 of the 10 groups for one sampling cap and one pad each.
In TOUCHSENSING, set TSLPRM_TOTAL_TOUCHKEYS_B to 8 and select the corresponding keys below this parameter.
Upon code generation, the tsl_user.h header file contains:
extern CONST TSL_TouchKey_T MyTKeys[];and the tsl_user.c source file contains:
/* TouchKeys list (ROM) */
CONST TSL_TouchKeyB_T MyTKeysB[TSLPRM_TOTAL_TOUCHKEYS_B] =
{
{ &MyTKeys_Data[0], &MyTKeys_Param[0], &MyChannels_Data[CHANNEL_0_DEST] },
{ &MyTKeys_Data[1], &MyTKeys_Param[1], &MyChannels_Data[CHANNEL_1_DEST] },
{ &MyTKeys_Data[2], &MyTKeys_Param[2], &MyChannels_Data[CHANNEL_2_DEST] },
{ &MyTKeys_Data[3], &MyTKeys_Param[3], &MyChannels_Data[CHANNEL_3_DEST] },
{ &MyTKeys_Data[4], &MyTKeys_Param[4], &MyChannels_Data[CHANNEL_4_DEST] },
{ &MyTKeys_Data[5], &MyTKeys_Param[5], &MyChannels_Data[CHANNEL_5_DEST] },
{ &MyTKeys_Data[6], &MyTKeys_Param[6], &MyChannels_Data[CHANNEL_6_DEST] },
{ &MyTKeys_Data[7], &MyTKeys_Param[7], &MyChannels_Data[CHANNEL_7_DEST] }
};meaning that when I attempt to access MyTKeysB in main.c using something like
#include "tsl.h"
#include "tsl_user.h"
MyTKeysB[i].p_Data->StateIdthe compiler returns
../Core/Src/main.c:514:13: error: 'MyTKeysB' undeclared (first use in this function); did you mean 'MyTKeys'?
514 | if (MyTKeysB[i].p_Data->StateId == TSL_STATEID_DETECT ||
| ^~~~~~~~
| MyTKeys
../Core/Src/main.c:514:13: note: each undeclared identifier is reported only once for each function it appears in
make: *** [Core/Src/subdir.mk:40: Core/Src/main.o] Error 1
make: *** Waiting for unfinished jobs....
However, if I then manually change the line in tsl_user.h to
extern CONST TSL_TouchKeyB_T MyTKeysB[];the code runs as expected and the basic touch keys work properly.
I don't have another machine to try this on right now, but I've been able to reproduce this issue on demand on my machine. Perhaps someone can confirm.
Thanks!
Solved! Go to Solution.
2025-05-29 9:21 AM
Hello @h7-v
Behavior reproduced and escalated internally (under internal ticket number 211146).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-26 1:13 PM
Hello @h7-v and welcome to the ST Community.
Thank you so much for reporting this. Could you please upload your .ioc file here for test.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-26 4:12 PM
Hi STTwo,
Thanks! Here's a fresh project .ioc using default parameters when asked on project creation. It has only two basic touch keys configured but the code generation exhibits the same behaviour between the tsl_user header and source files.
Let me know if you need anything else.
Cheers!
2025-05-29 9:21 AM
Hello @h7-v
Behavior reproduced and escalated internally (under internal ticket number 211146).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-29 11:03 AM
Fantastic. Glad this could be useful!
Cheers