2024-07-02 1:06 AM
Hey all,
i need to use the Rust Programming Language. Now i want to enable the PLL to increase the system srequency.
I'm using the "stm32h5" crate (https://crates.io/crates/stm32h5).
let dp = stm32h563::Peripherals::take().unwrap(); // Setup handler for device peripherals
let rcc = dp.RCC;
dp.FLASH.acr().write(|w| unsafe {
w.latency().bits(5);
w.prften().set_bit()
});
dp.PWR.voscr().write(|w| w.vos().bits(0b11)); //VOS scale 1
while dp.PWR.vossr().read().vosrdy().bit() != true {}
dp.ICACHE.cr().write(|w| w.en().set_bit());
rcc.cr().write(|w| w.hsebyp().set_bit());
rcc.cr().write(|w| w.hseon().set_bit()); //Enable High speed external clock 8 MHz
while rcc.cr().read().hserdy().bit_is_clear() {}
rcc.cr().write(|w| w.hseext().set_bit());
//PLL1
rcc.cr().write(|w| w.pll1on().clear_bit());
while rcc.cr().read().pll1rdy().bit_is_set() {}
rcc.pll1cfgr().write(|w| w.pll1src().bits(0b11)); //HSI as PLL1 source
rcc.pll1cfgr().write(|w| unsafe { w.pll1m().bits(4) }); //'16' for HSI
rcc.pll1divr()
.write(|w| unsafe { w.pll1n().bits(249).pll1p().bits(1).pll1q().bits(1) }); //250 MHz
rcc.pll1fracr().write(|w| w.pll1fracn().bits(0));
rcc.pll1cfgr().write(|w| w.pll1fracen().set_bit());
rcc.pll1cfgr().write(|w| w.pll1rge().bits(0b01)); //input frequency range 2 MHz to 4 MHz
rcc.pll1cfgr().write(|w| w.pll1vcosel().clear_bit()); //output frequency wide VCO range
rcc.pll1cfgr().write(|w| w.pll1pen().set_bit());
rcc.pll1cfgr().write(|w| w.pll1qen().set_bit());
rcc.cr().write(|w| w.pll1on().set_bit());
while rcc.cr().read().pll1rdy().bit_is_clear() {} //Stuck here
Does anybody know, what i'm doing wrong? Coudn't find any solutions so far.
Thanks
2024-07-02 1:42 AM
The command in line 23 is wrong. The HSE is the source, but the bits are right
2024-07-02 2:06 AM
Why are you enabling the fractional mode, when you program the integer mode (RCC_PLL1DIVR) from the PLL?
rcc.pll1fracr().write(|w| w.pll1fracn().bits(0)); rcc.pll1cfgr().write(|w| w.pll1fracen().set_bit());
The initialization flow according the TRM:
2024-07-02 2:23 AM
Hey Krotti42, thanks for your message.
I need the PLL for the FDCAN peripheral. For that i found an example here https://github.com/STMicroelectronics/STM32CubeH5/tree/main/Projects/NUCLEO-H563ZI/Examples/FDCAN
/*-------------------------------- PLL1 Configuration -----------------------*/
/* Check the parameters */
assert_param(IS_RCC_PLL(pOscInitStruct->PLL.PLLState));
if ((pOscInitStruct->PLL.PLLState) != RCC_PLL_NONE)
{
/* Check if the PLL1 is used as system clock or not */
if (temp_sysclksrc != RCC_SYSCLKSOURCE_STATUS_PLLCLK)
{
if ((pOscInitStruct->PLL.PLLState) == RCC_PLL_ON)
{
/* Check the parameters */
assert_param(IS_RCC_PLL1_SOURCE(pOscInitStruct->PLL.PLLSource));
assert_param(IS_RCC_PLL1_DIVM_VALUE(pOscInitStruct->PLL.PLLM));
assert_param(IS_RCC_PLL1_MULN_VALUE(pOscInitStruct->PLL.PLLN));
assert_param(IS_RCC_PLL1_DIVP_VALUE(pOscInitStruct->PLL.PLLP));
assert_param(IS_RCC_PLL1_DIVQ_VALUE(pOscInitStruct->PLL.PLLQ));
assert_param(IS_RCC_PLL1_DIVR_VALUE(pOscInitStruct->PLL.PLLR));
/* Disable the PLL1. */
__HAL_RCC_PLL1_DISABLE();
/* Get Start Tick*/
tickstart = HAL_GetTick();
/* Wait till PLL1 is disabled */
while (READ_BIT(RCC->CR, RCC_CR_PLL1RDY) != 0U)
{
if ((HAL_GetTick() - tickstart) > RCC_PLL_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}
/* Configure the PLL1 clock source, multiplication and division factors. */
__HAL_RCC_PLL1_CONFIG(pOscInitStruct->PLL.PLLSource,
pOscInitStruct->PLL.PLLM,
pOscInitStruct->PLL.PLLN,
pOscInitStruct->PLL.PLLP,
pOscInitStruct->PLL.PLLQ,
pOscInitStruct->PLL.PLLR);
assert_param(IS_RCC_PLL1_FRACN_VALUE(pOscInitStruct->PLL.PLLFRACN));
/* Disable PLL1FRACN . */
__HAL_RCC_PLL1_FRACN_DISABLE();
/* Configure PLL PLL1FRACN */
__HAL_RCC_PLL1_FRACN_CONFIG(pOscInitStruct->PLL.PLLFRACN);
/* Enable PLL1FRACN . */
__HAL_RCC_PLL1_FRACN_ENABLE();
assert_param(IS_RCC_PLL1_VCIRGE_VALUE(pOscInitStruct->PLL.PLLRGE));
/* Select PLL1 input reference frequency range: VCI */
__HAL_RCC_PLL1_VCIRANGE(pOscInitStruct->PLL.PLLRGE) ;
assert_param(IS_RCC_PLL1_VCORGE_VALUE(pOscInitStruct->PLL.PLLVCOSEL));
/* Select PLL1 output frequency range : VCO */
__HAL_RCC_PLL1_VCORANGE(pOscInitStruct->PLL.PLLVCOSEL) ;
/* Enable PLL1 System Clock output. */
__HAL_RCC_PLL1_CLKOUT_ENABLE(RCC_PLL1_DIVP);
/* Enable the PLL1. */
__HAL_RCC_PLL1_ENABLE();
/* Get Start Tick*/
tickstart = HAL_GetTick();
/* Wait till PLL1 is ready */
while (READ_BIT(RCC->CR, RCC_CR_PLL1RDY) == 0U)
{
if ((HAL_GetTick() - tickstart) > RCC_PLL_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}
}
And here they used the fractional value = 0 (as you can see in line 49). So i thought i could give it a try, but still won't work. Now I deleted this 2 lines out of my code, but noting changed.
2024-07-18 6:00 AM
Hello
If I understand correctly, you are using directly the STM32H5 Peripheral Access Crate because there is not yet an STM32H5 Rust HAL that provides high level clock configuration functions ?
The STM32H5 Rust HAL is very new and under development. There may be ongoing pull requests on the github project that could give you hints, even if they are not yet officially merged in a HAL release:
Guillaume