NetXDuo Secure X509 TLS Certificate not parsing
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-07-27 2:59 PM
Hi, I'm having issues getting self-signed certificates to work with NetXDuo Secure.
I started with the MQTT Secure Example which uses a mosquitto.org certificate and that works fine. However if I try to replace the mosquitto certificate with my own generated using OpenSSL, it's not accepted and nx_secure_x509_certificate_initialize returns invalid. Digging further into the source code, the actual error is in _nx_secure_x509_extract_oid_data which returns NX_SECURE_X509_FOUND_NON_ZERO_PADDING when extracting the RSA Bitstream.
Comparing my own certificates with the mosquitto.org one doesn't give any obvious clues and I don't know enough about the structure of binary DER encoded certificates to delve any deeper at the moment.
Does anyone have a 'known good' set of OpenSSL commands which generates a certificate which will parse successfully in NetXDuo please?
- Labels:
-
AzureRTOS
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-14 6:28 AM
Hi @Chris_GHSquared ,
Could you try the command:
$> openssl rsautl -encrypt -raw ...
According to the openssl documentation the '-raw' option allows generation of the certificates without padding.
regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-15 4:13 AM
Hi,
Thank you for your reply, I have been looking through all the openssl documentation and had found some references to padding but none of them seem to be applicable to the commands I'm using to generate a certificate. The process I'm using is:
#Generate key (-traditional forces PKCS#1, no encryption, I have also tried with -des3 and without the -traditional with same results)
openssl genrsa -traditional -out mqtt.key 2048
#Create CSR
openssl req -key mqtt.key -new -out mqtt.csr
# Create self-signed certificate
openssl x509 -signkey mqtt.key -in mqtt.csr -req -days 365 -out mqtt.crt
#Output in DER format
openssl x509 -in mqtt.crt -outform der -out mqtt.der
It is of course possible that I'm creating entirely the wrong type of certificate for the application.