NetxDuo not working with a static IP addresss
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-14 4:46 AM
Solved! Go to Solution.
- Labels:
-
Ethernet
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-22 4:35 PM
Hi @CharterWim
I'm just starting to learn ThreadX + NetXDuo, so I may have made a mistake that I'm still not aware of.
However, it seems I managed to run the Nx_UDP_Echo_Server without the debugger connected to my NUCLEO-H563ZI.
What I did was:
1. Disabled DHCP client exactly as you did.
2. When creating the UDP thread, I still used the TX_DONT_START so it will not run until asked to.
3. I changed the code in App_Link_Thread_Entry (app_netxduo.c) that verifies whether the cable is connected. Basically, I am calling nx_ip_driver_direct_command independent of the status returned by nx_ip_interface_status_check. I'm also using tx_thread_resume(&AppUDPThread) and tx_thread_suspend(&AppUDPThread) when the link is on or off. See my file attached. Seems to work.
Please let me know if I made any mistake, or if this works for you also!
BR
Fabio
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-14 11:04 AM
Hello @CharterWim ,
if you are regenerating with cubeMX and disabling DHCP addons it should compile and the includes should eliminated automatically.
You will find attached the file app_netxduo.c used to implement UDP Server with static IP.
BR
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-15 1:03 AM
Hi @STea,
Thank you for your swift response.
The "nxd_dhcp_client.h" include is not removed automatically by CubeMx when disabeling the DHCP client.
I think this is because it is inside a USER CODE section in the demo application code.
But this is not a big problem for me. I just wanted to be very detailed in describing what I did- and didn't do.
Unfortunately your app_netxduo.c yields the same results as my code.
It works when the debugger is attached.
It doesn't work when running without a debugger attached.
Yesterday I tried the same demo application from an older version of the MCU package, STM32Cube_FW_H5_V1.1.1 instead of STM32Cube_FW_H5_V1.2.0.
In the older package, the demo app does work with a static IP address without the debugger attached.
I got the idea after reading this thread about a problem simular to the one I'm facing.
There appears to be something wrong with the STM32Cube_FW_H5_V1.2.0 package I think.
Unfortunately it is hard to use STM32Cube_FW_H5_V1.1.1 with CubeMX.
Even after I removed the STM32Cube_FW_H5_V1.2.0 package, it does not want to generate code with version V1.1.1.
It keeps downloading V1.2.0
Is there a way to work around this?
Or (better even) do you have an ETA on when the problem in the MCU package will be solved? (Internal ticket number: 179408)
Regards, Wim!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-15 10:02 AM
Hello @CharterWim ,
the ticket is still in progress indeed your problem is related to the same issue. you will get some updates soon as our experts are analyzing the root cause.
BR
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-22 4:35 PM
Hi @CharterWim
I'm just starting to learn ThreadX + NetXDuo, so I may have made a mistake that I'm still not aware of.
However, it seems I managed to run the Nx_UDP_Echo_Server without the debugger connected to my NUCLEO-H563ZI.
What I did was:
1. Disabled DHCP client exactly as you did.
2. When creating the UDP thread, I still used the TX_DONT_START so it will not run until asked to.
3. I changed the code in App_Link_Thread_Entry (app_netxduo.c) that verifies whether the cable is connected. Basically, I am calling nx_ip_driver_direct_command independent of the status returned by nx_ip_interface_status_check. I'm also using tx_thread_resume(&AppUDPThread) and tx_thread_suspend(&AppUDPThread) when the link is on or off. See my file attached. Seems to work.
Please let me know if I made any mistake, or if this works for you also!
BR
Fabio
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-23 4:03 AM