Skip to main content
BViet.1
Associate III
Apr 18, 2024 12:46 PM UTC
Solved

[STM32H563] NetXDuo TCP Echo Server only working in Debug mode (fixed IP address)

Hi :)

I have a custom board where I need to use the ethernet interface. Starting with a NUCLEO-H563ZI I ported the NetXDuo TCP Server Echo example to my board.

When I'm using the example as expected with a DHCP server connected (e.g. ethernet connection to a router or switch) then everything works. I can use the board in debug mode or in release mode. 

My goal is to connect the board directly to my Mac (or any other laptop) and assign a fixed IP address to the MCU. This works fine when I'm in a debugging session. In release mode I cannot establish a connection as a TCP client.

Does anybody has an idea how to find the problem?

As you can see in the following code of app_netxduo.c I just removed the DHCP things in the CubeMX configuration and added the IP address and net mask.

"app_netxduo.h"

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file app_netxduo.h
 * @author MCD Application Team
 * @brief NetXDuo applicative header file
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Define to prevent recursive inclusion -------------------------------------*/
#ifndef __APP_NETXDUO_H__
#define __APP_NETXDUO_H__

#ifdef __cplusplus
extern "C" {
#endif

/* Includes ------------------------------------------------------------------*/
#include "nx_api.h"

/* Private includes ----------------------------------------------------------*/
#include "nx_stm32_eth_driver.h"

/* USER CODE BEGIN Includes */
#include "main.h"
/* USER CODE END Includes */

/* Exported types ------------------------------------------------------------*/
/* USER CODE BEGIN ET */

/* USER CODE END ET */

/* Exported constants --------------------------------------------------------*/
/* USER CODE BEGIN EC */

/* USER CODE END EC */
/* The DEFAULT_PAYLOAD_SIZE should match with RxBuffLen configured via MX_ETH_Init */
#ifndef DEFAULT_PAYLOAD_SIZE
#define DEFAULT_PAYLOAD_SIZE 1536
#endif

#ifndef DEFAULT_ARP_CACHE_SIZE
#define DEFAULT_ARP_CACHE_SIZE 1024
#endif

/* Exported macro ------------------------------------------------------------*/
/* USER CODE BEGIN EM */
#define PRINT_IP_ADDRESS(addr) do { \
 printf("STM32 %s: %lu.%lu.%lu.%lu \n", #addr, \
 (addr >> 24) & 0xff, \
 (addr >> 16) & 0xff, \
 (addr >> ‌8)‌ & 0xff, \
 addr& 0xff);\
 }while(0)

#define PRINT_DATA(addr, port, data) do { \
 printf("[%lu.%lu.%lu.%lu:%u] -> '%s' \n", \
 (addr >> 24) & 0xff, \
 (addr >> 16) & 0xff, \
 (addr >> ‌8)‌ & 0xff, \
 (addr & 0xff), port, data); \
 } while(0)
/* USER CODE END EM */

/* Exported functions prototypes ---------------------------------------------*/
UINT MX_NetXDuo_Init(VOID *memory_ptr);

/* USER CODE BEGIN EFP */

/* USER CODE END EFP */

/* Private defines -----------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define DEFAULT_MEMORY_SIZE 1024
#define DEFAULT_PRIORITY 10
#define WINDOW_SIZE 512
#define LINK_PRIORITY 11
#define NULL_ADDRESS 0
#define DEFAULT_PORT 6000
#define MAX_TCP_CLIENTS 1
/* USER CODE END PD */

#define NX_APP_DEFAULT_TIMEOUT (10 * NX_IP_PERIODIC_RATE)

#define NX_APP_PACKET_POOL_SIZE ((DEFAULT_PAYLOAD_SIZE + sizeof(NX_PACKET)) * 10)

#define NX_APP_THREAD_STACK_SIZE 2*1024

#define Nx_IP_INSTANCE_THREAD_SIZE 2*1024

#define NX_APP_THREAD_PRIORITY 10

#ifndef NX_APP_INSTANCE_PRIORITY
#define NX_APP_INSTANCE_PRIORITY NX_APP_THREAD_PRIORITY
#endif

#define NX_APP_DEFAULT_IP_ADDRESS IP_ADDRESS(192, 168, 1, 32)

#define NX_APP_DEFAULT_NET_MASK IP_ADDRESS(255, 255, 255, 0)

/* USER CODE BEGIN 1 */

/* USER CODE END 1 */

#ifdef __cplusplus
}
#endif
#endif /* __APP_NETXDUO_H__ */

 

"app_netxduo.c"

 

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file app_netxduo.c
 * @author MCD Application Team
 * @brief NetXDuo applicative file
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/
#include "app_netxduo.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "nx_stm32_eth_config.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* Define Threadx global data structures. */
TX_THREAD AppTCPThread;
TX_THREAD AppLinkThread;
/* Define NetX global data structures. */
ULONG IpAddress;
ULONG NetMask;
NX_TCP_SOCKET TCPSocket;
/* App memory pointer. */
CHAR *pointer;
/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
TX_THREAD NxAppThread;
NX_PACKET_POOL NxAppPool;
NX_IP NetXDuoEthIpInstance;
/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
static VOID nx_app_thread_entry (ULONG thread_input);
/* USER CODE BEGIN PFP */
/* TCP thread entry */
static VOID App_TCP_Thread_Entry(ULONG thread_input);
/* Link thread entry */
static VOID App_Link_Thread_Entry(ULONG thread_input);
static VOID tcp_listen_callback(NX_TCP_SOCKET *socket_ptr, UINT port);
static void tcp_disconnect_callback(NX_TCP_SOCKET *socket_ptr);
/* USER CODE END PFP */

/**
 * @brief Application NetXDuo Initialization.
 * memory_ptr: memory pointer
 * @retval int
 */
UINT MX_NetXDuo_Init(VOID *memory_ptr)
{
 UINT ret = NX_SUCCESS;
 TX_BYTE_POOL *byte_pool = (TX_BYTE_POOL*)memory_ptr;

 /* USER CODE BEGIN App_NetXDuo_MEM_POOL */
 (void)byte_pool;
 /* USER CODE END App_NetXDuo_MEM_POOL */
 /* USER CODE BEGIN 0 */

 /* USER CODE END 0 */

 /* Initialize the NetXDuo system. */
 CHAR *pointer;
 nx_system_initialize();

 /* Allocate the memory for packet_pool. */
 if (tx_byte_allocate(byte_pool, (VOID **) &pointer, NX_APP_PACKET_POOL_SIZE, TX_NO_WAIT) != TX_SUCCESS)
 {
 return TX_POOL_ERROR;
 }

 /* Create the Packet pool to be used for packet allocation,
 * If extra NX_PACKET are to be used the NX_APP_PACKET_POOL_SIZE should be increased
 */
 ret = nx_packet_pool_create(&NxAppPool, "NetXDuo App Pool", DEFAULT_PAYLOAD_SIZE, pointer, NX_APP_PACKET_POOL_SIZE);

 if (ret != NX_SUCCESS)
 {
 return NX_POOL_ERROR;
 }

 /* Allocate the memory for Ip_Instance */
 if (tx_byte_allocate(byte_pool, (VOID **) &pointer, Nx_IP_INSTANCE_THREAD_SIZE, TX_NO_WAIT) != TX_SUCCESS)
 {
 return TX_POOL_ERROR;
 }

 /* Create the main NX_IP instance */
 ret = nx_ip_create(&NetXDuoEthIpInstance, "NetX Ip instance", NX_APP_DEFAULT_IP_ADDRESS, NX_APP_DEFAULT_NET_MASK, &NxAppPool, nx_stm32_eth_driver,
 pointer, Nx_IP_INSTANCE_THREAD_SIZE, NX_APP_INSTANCE_PRIORITY);

 if (ret != NX_SUCCESS)
 {
 return NX_NOT_SUCCESSFUL;
 }

 /* Allocate the memory for ARP */
 if (tx_byte_allocate(byte_pool, (VOID **) &pointer, DEFAULT_ARP_CACHE_SIZE, TX_NO_WAIT) != TX_SUCCESS)
 {
 return TX_POOL_ERROR;
 }

 /* Enable the ARP protocol and provide the ARP cache size for the IP instance */

 /* USER CODE BEGIN ARP_Protocol_Initialization */

 /* USER CODE END ARP_Protocol_Initialization */

 ret = nx_arp_enable(&NetXDuoEthIpInstance, (VOID *)pointer, DEFAULT_ARP_CACHE_SIZE);

 if (ret != NX_SUCCESS)
 {
 return NX_NOT_SUCCESSFUL;
 }

 /* Enable the ICMP */

 /* USER CODE BEGIN ICMP_Protocol_Initialization */

 /* USER CODE END ICMP_Protocol_Initialization */

 ret = nx_icmp_enable(&NetXDuoEthIpInstance);

 if (ret != NX_SUCCESS)
 {
 return NX_NOT_SUCCESSFUL;
 }

 /* Enable TCP Protocol */

 /* USER CODE BEGIN TCP_Protocol_Initialization */

 /* USER CODE END TCP_Protocol_Initialization */

 ret = nx_tcp_enable(&NetXDuoEthIpInstance);

 if (ret != NX_SUCCESS)
 {
 return NX_NOT_SUCCESSFUL;
 }

 /* Allocate the memory for main thread */
 if (tx_byte_allocate(byte_pool, (VOID **) &pointer, NX_APP_THREAD_STACK_SIZE, TX_NO_WAIT) != TX_SUCCESS)
 {
 return TX_POOL_ERROR;
 }

 /* Create the main thread */
 ret = tx_thread_create(&NxAppThread, "NetXDuo App thread", nx_app_thread_entry , 0, pointer, NX_APP_THREAD_STACK_SIZE,
 NX_APP_THREAD_PRIORITY, NX_APP_THREAD_PRIORITY, TX_NO_TIME_SLICE, TX_AUTO_START);

 if (ret != TX_SUCCESS)
 {
 return TX_THREAD_ERROR;
 }

 /* USER CODE BEGIN MX_NetXDuo_Init */
 /* Allocate the memory for TCP server thread */
 if (tx_byte_allocate(byte_pool, (VOID **) &pointer,2 * DEFAULT_MEMORY_SIZE, TX_NO_WAIT) != TX_SUCCESS)
 {
 return TX_POOL_ERROR;
 }

 /* create the TCP server thread */
 ret = tx_thread_create(&AppTCPThread, "App TCP Thread", App_TCP_Thread_Entry, 0, pointer, 2 * DEFAULT_MEMORY_SIZE,
 DEFAULT_PRIORITY, DEFAULT_PRIORITY, TX_NO_TIME_SLICE, TX_DONT_START);

 if (ret != TX_SUCCESS)
 {
 return TX_THREAD_ERROR;
 }

 /* Allocate the memory for Link thread */
 if (tx_byte_allocate(byte_pool, (VOID **) &pointer,2 * DEFAULT_MEMORY_SIZE, TX_NO_WAIT) != TX_SUCCESS)
 {
 return TX_POOL_ERROR;
 }

 /* create the Link thread */
 ret = tx_thread_create(&AppLinkThread, "App Link Thread", App_Link_Thread_Entry, 0, pointer, 2 * DEFAULT_MEMORY_SIZE,
 LINK_PRIORITY, LINK_PRIORITY, TX_NO_TIME_SLICE, TX_AUTO_START);

 if (ret != TX_SUCCESS)
 {
 return TX_THREAD_ERROR;
 }
 /* USER CODE END MX_NetXDuo_Init */

 return ret;
}

/**
* @brief Main thread entry.
* thread_input: ULONG user argument used by the thread entry
* @retval none
*/
static VOID nx_app_thread_entry (ULONG thread_input)
{
 /* USER CODE BEGIN Nx_App_Thread_Entry 0 */
 UINT ret = NX_SUCCESS;

 ret = nx_ip_address_get(&NetXDuoEthIpInstance, &IpAddress, &NetMask);

 /* print the IP address and the net mask */
 PRINT_IP_ADDRESS(IpAddress);

 if (ret != TX_SUCCESS)
 {
 Error_Handler();
 }

 /* the network is correctly initialized, start the TCP server thread */
 tx_thread_resume(&AppTCPThread);

 /* this thread is not needed any more, we relinquish it */
 tx_thread_relinquish();
 /* USER CODE END Nx_App_Thread_Entry 0 */

}
/* USER CODE BEGIN 1 */
/**
* @brief TCP listen call back
* socket_ptr: NX_TCP_SOCKET socket registered for the callback
* port: UINT the port on which the socket is listening
* @retval none
*/
static VOID tcp_listen_callback(NX_TCP_SOCKET *socket_ptr, UINT port)
{
 /* as soon as the IP address is ready, the semaphore is released */
// tx_semaphore_put(&DHCPSemaphore);
 HAL_GPIO_WritePin(LED_USER2_GPIO_Port, LED_USER2_Pin, GPIO_PIN_SET);
 printf("--- TCP_LISTEN_CALLBACK ---\n");
}

static void tcp_disconnect_callback(NX_TCP_SOCKET *socket_ptr)
{
 HAL_GPIO_WritePin(LED_USER2_GPIO_Port, LED_USER2_Pin, GPIO_PIN_RESET);
 printf("--- TCP_DISCONNECT_CALLBACK ---\n");
}

/**
* @brief TCP server thread entry
* thread_input: ULONG thread parameter
* @retval none
*/
static VOID App_TCP_Thread_Entry(ULONG thread_input)
{
 UINT ret;
 UCHAR data_buffer[512];

 ULONG source_ip_address;
 NX_PACKET *data_packet;

 UINT source_port;
 ULONG bytes_read;

 /* create the TCP socket */
 ret = nx_tcp_socket_create(&NetXDuoEthIpInstance, &TCPSocket, "TCP Server Socket", NX_IP_NORMAL, NX_FRAGMENT_OKAY,
 NX_IP_TIME_TO_LIVE, WINDOW_SIZE, tcp_disconnect_callback, NX_NULL);
 if (ret)
 {
 Error_Handler();
 }

 /*
 * listen to new client connections.
 * the TCP_listen_callback will release the 'Semaphore' when a new connection is available
 */
 ret = nx_tcp_server_socket_listen(&NetXDuoEthIpInstance, DEFAULT_PORT, &TCPSocket, MAX_TCP_CLIENTS, tcp_listen_callback);

 if (ret)
 {
 Error_Handler();
 }
 else
 {
 printf("TCP Server listening on PORT %d ..\n", DEFAULT_PORT);
 }

 /* accept the new client connection before starting data exchange */
 ret = nx_tcp_server_socket_accept(&TCPSocket, TX_WAIT_FOREVER);

 if (ret)
 {
 Error_Handler();
 }

 while(1)
 {
 ULONG socket_state;

 TX_MEMSET(data_buffer, '\0', sizeof(data_buffer));

 /* get the socket state */
 nx_tcp_socket_info_get(&TCPSocket, NULL, NULL, NULL, NULL, NULL, NULL, NULL, &socket_state, NULL, NULL, NULL);

 /* if the connections is not established then accept new ones, otherwise start receiving data */
 if(socket_state != NX_TCP_ESTABLISHED)
 {
 printf("Waiting for TCP client\n");
 ret = nx_tcp_server_socket_accept(&TCPSocket, NX_IP_PERIODIC_RATE);
 }

 if(ret == NX_SUCCESS)
 {
 printf("Connection established\n");
 /* receive the TCP packet send by the client */
 ret = nx_tcp_socket_receive(&TCPSocket, &data_packet, NX_WAIT_FOREVER);

 if (ret == NX_SUCCESS)
 {
 HAL_GPIO_TogglePin(LED_USER2_GPIO_Port, LED_USER2_Pin);

 /* get the client IP address and port */
 nx_udp_source_extract(data_packet, &source_ip_address, &source_port);

 /* retrieve the data sent by the client */
 nx_packet_data_retrieve(data_packet, data_buffer, &bytes_read);

 /* print the received data */
 PRINT_DATA(source_ip_address, source_port, data_buffer);

 /* immediately resend the same packet */
 ret = nx_tcp_socket_send(&TCPSocket, data_packet, NX_IP_PERIODIC_RATE);

 if (ret == NX_SUCCESS)
 {
 HAL_GPIO_TogglePin(LED_USER2_GPIO_Port, LED_USER2_Pin);
 }
 }
 else
 {
 nx_tcp_socket_disconnect(&TCPSocket, NX_WAIT_FOREVER);
 nx_tcp_server_socket_unaccept(&TCPSocket);
 nx_tcp_server_socket_relisten(&NetXDuoEthIpInstance, DEFAULT_PORT, &TCPSocket);
 }
 }
 else
 {
 /*toggle the green led to indicate the idle state */
// HAL_GPIO_TogglePin(LED_USER2_GPIO_Port, LED_USER2_Pin);
 }
 }
}

/**
* @brief Link thread entry
* thread_input: ULONG thread parameter
* @retval none
*/
static VOID App_Link_Thread_Entry(ULONG thread_input)
{
 ULONG actual_status;
 UINT linkdown = 0, status;

 while(1)
 {
 /* Get Physical Link stackavailtus. */
 status = nx_ip_interface_status_check(&NetXDuoEthIpInstance, 0, NX_IP_LINK_ENABLED,
 &actual_status, 10);

 if(status == NX_SUCCESS)
 {
 if(linkdown == 1)
 {
 linkdown = 0;
 status = nx_ip_interface_status_check(&NetXDuoEthIpInstance, 0, NX_IP_ADDRESS_RESOLVED,
 &actual_status, 10);
 if(status == NX_SUCCESS)
 {
 /* The network cable is connected again. */
 printf("The network cable is connected again.\n");
 /* Print TCP Echo Server is available again. */
 printf("TCP Echo Server is available again.\n");
 }
 else
 {
 /* The network cable is connected. */
 printf("The network cable is connected.\n");
 /* Send command to Enable Nx driver. */
 nx_ip_driver_direct_command(&NetXDuoEthIpInstance, NX_LINK_ENABLE,
 &actual_status);
 }
 }
 }
 else
 {
 if(0 == linkdown)
 {
 linkdown = 1;
 /* The network cable is not connected. */
 printf("The network cable is not connected.\n");
 }
 }

 tx_thread_sleep(NX_ETH_CABLE_CONNECTION_CHECK_PERIOD);
 }
}
/* USER CODE END 1 */

 

 

 

 

This topic has been closed for replies.
zeitgeist
zeitgeistBest answer
Associate
Sep 12, 2024 12:41 PM UTC

Hello @STea,

I found the problem that it seems NUCLEO-H563ZI's Ethernet circuit (LAN8742) is designed to work with STLINK only(what i mean is lan8742 can not have reset without ST-LINK)

How to reproduce:

It does not work with external power supply, because NRST is only connected to the STLINK, If NUCLEO-H563ZI only supplied with external power supply but nothing else at initial power, it does not work.

If you connect STLINK while powering the board externally and try debugging it, it will work. 

I dont know if there is a jumper resistor to switch LAN8742's nRST to a GPIO. 

Im trying to work around this problem. 

 

 

7 replies

BViet.1
BViet.1Author
Associate III
Apr 19, 2024 2:26 PM UTC

I figured out that the problem is related to 
https://community.st.com/t5/stm32-mcus-embedded-software/h5-1-2-0-and-cube-1-5-break-ethernet/td-p/653320
and
https://community.st.com/t5/stm32-mcus-embedded-software/netxduo-issues-after-power-loss/td-p/661479

With STM32CubeIDE v1.14.0 it works as expected without debugger and also after switching the power supply.

ST Employee
Apr 23, 2024 9:38 AM UTC

Hello @BViet.1 ,

This is indeed related to the threads you mentioned I'll try to keep you in touch with the updates on this case.

BR 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
zeitgeist
Associate
Sep 6, 2024 1:19 PM UTC

Hello STea,

I am facing the same issue. Im using IAR EWARM,  Project was built with STM32CubeMX V6.8.0 using STM32Cube FW_H5 V1.0.1. Im using NUCLEO-H563ZI and NetXDuo TCP Echo Server.DHCP is disabled.

Works at Debug mode, does not work after exiting debug and re-powering the board.

Tried my best to solve this, searched every forum but still could not find any answer.

 

Graduate
May 25, 2024 5:16 PM UTC

Hi @BViet.1!

Please take a look at https://community.st.com/t5/stm32-mcus-embedded-software/netxduo-not-working-with-a-static-ip-addresss/td-p/673975. Maybe the issue you are having is the same as there.

 

Please let me know if that is a solution for you.

BR,

FabioFly