cancel
Showing results for 
Search instead for 
Did you mean: 

mss for netXduo Webserver

AZorn.1
Associate III

Hello,
i am using ThreadX and NetXduo for an ethernet applikation.

For this i need several tcp connections, all with reduced mss to about 900bytes. So i configured each socket with the nx_tcp_socket_mss_set(...) function after socketCreate, as it is supposed i guess.

So far so good, all things are working, also with reduced packet size in nx-pools.

But to the question, i also need webserver running, and therefor it is also necessary to reduce the mss, not to overshot the packetpool-size. How is this done, for the webserver sockets, as they can't be accesses through usercode.

Is it supposed to change the default mss in nx_tcp.h, as this is part of the library. I can't find any other "user" option to change mss for webserver-sockets, as to change the library-code.

is there anything else?

best regards

0 REPLIES 0