cancel
Showing results for 
Search instead for 
Did you mean: 

MQTT pbuf_free: p->ref > 0 error

cleonb322
Associate III

I am working on an STM32f767 project with LWIP and MQTT. Everything seemed to work for a while but eventually, I received the following assert:  "pbuf_free: p->ref > 0..." which caused it to crash sometimes; but sometimes it will continue to work without any issue.  Has anyone had a similar issue?

According to LWIP_IAP example, memory location 0x20048000 is labeled as ethernet rx buffer location; however, I could not find where this location is linked to the ethernet rx buffer. for example, 0x2007C000 memory location in the linker file for RxDescripSection & TxDecripSection. And does the size of the MPU region have to be equal to or greater than MEM_SIZE defined in opt.h?

 

My settings: 

LinkerScript.ld

Memory_B1(xrw) : ORIGIN = 0x2004C000, LENGTH = 0xA0

Memory_B2(xrw) : ORIGIN = 0x2004C0A0, LENGTH = 0xA0

 

.RxDecripSection (NOLOAD) : { *(.RxDescripSection) } >Memory_B1

.TxDecripSection (NOLOAD) : { *(.DMATxDscrTab_section) } >Memory_B2

.ARM.attributes 0 : { *(.ARM.attributes) }

 

main.c 

 

/* Configure the MPU as Normal Non Cacheable for Ethernet Buffers in the SRAM2 */

MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.BaseAddress = 0x20048000;
MPU_InitStruct.Size = MPU_REGION_SIZE_16KB;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER1;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1;
MPU_InitStruct.SubRegionDisable = 0x00;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;

HAL_MPU_ConfigRegion(&MPU_InitStruct);

 

/* Configure the MPU as Device for Ethernet Descriptors in the SRAM2 */
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.BaseAddress = 0x2004C000;
MPU_InitStruct.Size = MPU_REGION_SIZE_1KB;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER2;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.SubRegionDisable = 0x00;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE

HAL_MPU_ConfigRegion(&MPU_InitStruct);

 

1 ACCEPTED SOLUTION

Accepted Solutions
STea
ST Employee

Hello @cleonb322 ,

based on the example LwIP_HTTP_Server_Netconn_RTOS  your MPU configuration should be as follows as you are using an STM32F767 check RM0410

STea_0-1720191391274.png

static void MPU_Config(void) { MPU_Region_InitTypeDef MPU_InitStruct; /* Disable the MPU */ HAL_MPU_Disable(); /* Configure the MPU as Strongly ordered for not defined regions */ MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.BaseAddress = 0x00; MPU_InitStruct.Size = MPU_REGION_SIZE_4GB; MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS; MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER0; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; MPU_InitStruct.SubRegionDisable = 0x87; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /* Configure the MPU as Normal Non Cacheable for Ethernet Buffers in the SRAM2 */ MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.BaseAddress = 0x20078000; MPU_InitStruct.Size = MPU_REGION_SIZE_16KB; MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER1; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1; MPU_InitStruct.SubRegionDisable = 0x00; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /* Configure the MPU as Device for Ethernet Descriptors in the SRAM2 */ MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.BaseAddress = 0x2007C000; MPU_InitStruct.Size = MPU_REGION_SIZE_1KB; MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER2; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; MPU_InitStruct.SubRegionDisable = 0x00; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /* Enable the MPU */ HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT); }
View more

The MPU configuration you are using is valid for stm32f75xx and stm32f74xx check RM0385

STea_1-1720191644932.png


Regards

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
STea
ST Employee

Hello @cleonb322 ,

based on the example LwIP_HTTP_Server_Netconn_RTOS  your MPU configuration should be as follows as you are using an STM32F767 check RM0410

STea_0-1720191391274.png

static void MPU_Config(void) { MPU_Region_InitTypeDef MPU_InitStruct; /* Disable the MPU */ HAL_MPU_Disable(); /* Configure the MPU as Strongly ordered for not defined regions */ MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.BaseAddress = 0x00; MPU_InitStruct.Size = MPU_REGION_SIZE_4GB; MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS; MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER0; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; MPU_InitStruct.SubRegionDisable = 0x87; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /* Configure the MPU as Normal Non Cacheable for Ethernet Buffers in the SRAM2 */ MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.BaseAddress = 0x20078000; MPU_InitStruct.Size = MPU_REGION_SIZE_16KB; MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER1; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1; MPU_InitStruct.SubRegionDisable = 0x00; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /* Configure the MPU as Device for Ethernet Descriptors in the SRAM2 */ MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.BaseAddress = 0x2007C000; MPU_InitStruct.Size = MPU_REGION_SIZE_1KB; MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER2; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; MPU_InitStruct.SubRegionDisable = 0x00; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /* Enable the MPU */ HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT); }
View more

The MPU configuration you are using is valid for stm32f75xx and stm32f74xx check RM0385

STea_1-1720191644932.png


Regards

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
cleonb322
Associate III

Thank you for the help. it no longer crashes but I still receive "pbuf_free: p->ref > 0" occasionally on the debug console. Do you know of other potential causes of the issue?

Hello @cleonb322 ,

This most probably related to LWIP memory management and since it is not systematic maybe it can be a problem of alignment or luck of allocated memory.

As far as I recall there are two routes to manage memory in LWIP either dynamically or statically and this could be adjusted by the user.
have a look at sections 3.2 and 4 of UM1713 .

Regards

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I forget to update this:  #define LWIP_RAM_HEAP_POINTER (0x20078000) in iwapopts.h

I tried to enable TLS, but it failed malloc because MBEDTLS_SSL_IN_BUFFER_LEN size is 16717 and the available memory is 16K (16384) for SRAM2. according to TLS standards, I should not change the size of MBEDTLS_SSL_IN_BUFFER_LEN. what are my options? I have an external RAM on the device for display buffer with plenty of space available. is it possible to use the external RAM starting at memory location 0xC0000000?