2021-12-02 2:25 AM
Hi,
First I'm new to the STM environment.
I'm setting up the Board to test some stuff, with raw LwIP. I'm having a weird issue, where the board freezes when i plug in a connected ethernet cable.
I made no other changes (exept one, look below point 3)
Code (tcpecho_raw_init is from an example:(
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_LWIP_Init();
LED_timer = TCP_timouts_timer = HAL_GetTick();
tcpecho_raw_init();
while (1)
{
if (TCP_timouts_timer < HAL_GetTick())
{
sys_check_timeouts();
TCP_timouts_timer = HAL_GetTick() + 5;
}
if (LED_timer < HAL_GetTick())
{
HAL_GPIO_TogglePin(LED_PIN_GPIO_Port, LED_PIN_Pin);
LED_timer = HAL_GetTick() + 500;
}
HAL_Delay(1);
}
}
Board: Olimex STM32-E407 Rev.F
Toolchain: STM32CubeIDE + ST-Link v2
Thank you for your Help
Stefan
PS: Other Problems you could help me with: