2024-10-24 07:17 AM - last edited on 2024-10-24 07:35 AM by SofLit
Hi, i have STM32F767 and im using FreeRTOS V2 and lwIP. Im facing known bug which should be fixed in FW_F7 V1.17 and im using FW_F7 V1.17.2 and still facing this.
When i connect the ethernet cable, after 2 seconds FW is stuck at following place:
I tried to disable DHCP everyting is ok, but when i try to ping the board the result is the same.
Can you help me to solve this issue?
2024-10-24 08:12 AM
Hello @Petr3,
are you sure you are using the latest version of CubeFirmware as you can see that this fix is available on GitHub
Release v1.17.2 · STMicroelectronics/STM32CubeF7@767d083
in the new version the fix is as follows :
do
{
if(HAL_ETH_Transmit_IT(&EthHandle, &TxConfig) == HAL_OK)
{
errval = ERR_OK;
}
else
{
if(HAL_ETH_GetError(&EthHandle) & HAL_ETH_ERROR_BUSY)
{
/* Wait for descriptors to become available */
osSemaphoreWait( TxPktSemaphore, ETHIF_TX_TIMEOUT);
HAL_ETH_ReleaseTxPacket(&EthHandle);
errval = ERR_BUF;
}
else
{
/* Other error */
pbuf_free(p);
errval = ERR_IF;
}
}
}while(errval == ERR_BUF);
the fix is related to LWIP application and not Ethernet and it is present in V1.17.2 and here are the changes:
Regards
2024-10-24 08:57 AM
Hello STea,
i hope im using latest version of FW pack:
but the lwIP code seems to be different:
where i can update lwIP for latest version? I thought it is part of FW pack for F7 family.
2024-10-24 09:46 AM
Hello @Petr3 ,
you are right, the generated code with MX is generated with the old Ethernetif.c template I'm able to reproduce this and I reported it internally (ticket number 194996 internal reference only) for investigation
in the meanwhile, I suggest you make those changes to your code manually and you should be good to go.
Regards
2024-10-24 02:30 PM
Hello @STea ,
thank you for your quick answer. I'll try to edit Ethernetif.c manually but for now im often regenerating the code, so i can work on another part of my FW. Do you know, how much time take the invetigation and release fixed FW pack?
Regards