2026-04-09 5:29 AM - last edited on 2026-04-09 10:01 AM by mƎALLEm
NUCLEO-F767ZI
I'm trying to use the LwIP middleware which I have enabled in MX.
First I'm trying to check if an ethernet cable is attached or not. I have setup UART3 to use printf (which works as expected)
I've set the callback in lwip.c to print when the cable is removed or plugged in or so I thought but I get no message when I connect or disconnect the cable. The LEDs on the socket light up when the cable is connected, so the board at some level does see the cable. What am I missing here?
EDIT:: LWIP_NETIF_LINK_CALLBACK was enabled in MX
// In main.c
MX_LWIP_Init();
/* USER CODE BEGIN WHILE */
while (1)
{
MX_LWIP_Process();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
// In lwip.c the callback function that is registered in MX_LWIP_Init()
static void ethernet_link_status_updated(struct netif *netif)
{
if (netif_is_up(netif))
{
/* USER CODE BEGIN 5 */
printf("Cable connected\r\n");
/* USER CODE END 5 */
}
else /* netif is down */
{
/* USER CODE BEGIN 6 */
printf("Cable NOT connected\r\n");
/* USER CODE END 6 */
}
}
Solved! Go to Solution.
2026-04-09 8:45 AM - edited 2026-04-09 8:46 AM
Besides that stuff, what mbarg said: connection management.
The PHY must be read periodically (EthPhyLinkStatus() reads the PHY registers), otherwise how should LWIP know about any connection?
Something like this (not HAL, but you'll get the idea) is called in the loop / LwipProcess():
/**
* @brief This function sets the netif link status.
* @note This function should be included in the main loop to poll
* for the link status update
* @PAram pNetIf: pointer to the network interface
* @retval None
*/
void Ethernet_Link_Periodic_Handle(struct netif *pNetIf)
{
static uint32_t u32EthLinkTimer = 0;
/* check PHY ethernet link every 200 ms */
if( (HAL_GetTick() - u32EthLinkTimer) >= ETH_TIMEOUT_NETIF_LINK_PRD_HNDL_MS )
{
uint8_t u8LinkUp = 0;
u32EthLinkTimer = HAL_GetTick();
if( EthPhyLinkStatus(u8PhyPortActive, ETH_LINK_CHECK_QUICK) == HAL_OK ) u8LinkUp = 1;
/* check if the netif link down and the PHY link is up */
if( !netif_is_link_up(pNetIf) && (1 == u8LinkUp) )
{
/* network cable is connected */
netif_set_link_up(pNetIf);
}
else if( netif_is_link_up(pNetIf) && (0 == u8LinkUp) )
{
/* network cable is disconnected */
netif_set_link_down(pNetIf);
}
}
}
2026-04-13 2:29 AM - edited 2026-04-21 8:41 AM
@NicRoberts, have you managed to fix the Ethernet issue?
2026-04-23 6:25 AM - edited 2026-04-23 6:25 AM
Yes thankyou for your help, been busy week only just got a chance to test it. I followed the instructions in the link you posted & its all working now.
2026-04-23 6:26 AM
You are most welcome!