2024-03-15 9:41 AM
Heyho,
I'm about to start writing an ethernet bootloader for the H7.
I found the F7's LwIP_IAP example, a good way to get ideas how to realize the bootloader, although I'll probably put the new bin into an external SPI flash.
As I have an http-webserver with a few pages already up and running, I will use the http method.
The example is using LwIP's "standard" fs_data.c file containing the STM32's webpage, prepared with makefsdata.
But where can I find the original html-files which served as the fs_data source ?
I don't want to learn any more html, the webserver is more or less a debugging tool, so it would be a great help if I could simply modify the original html-files to fit my purpose.
Maybe @STea or @Peter BENSCH might help
Thanks in advance!
PS: I already checked the original F4 example on Github, no html there.
Solved! Go to Solution.
2024-12-18 12:31 AM
If you got the header of the POST message, then you will surely get the rest.
Read, check, think, try...
Check which httpd_post_* functions are called from httpd.c, but NOT implemented. Then search the web or build your own.