cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with srand() causing exit in STM32H747 Project with FreeRTOS and lwIP

OskarP
Associate III

Hello everyone,

I’m encountering an issue with the srand() function in my STM32H747 project, and I would appreciate your insights on what might be causing this problem.

Hardware:

  • MCU: STM32H747IIT6
  • Custom board

Software setup:

  • CubeMX-generated project
  • Cube CLT version: 1.17
  • Firmware version: 1.12.1

Problem Description

Whenever I call the srand() function, my code immediately ends up in the exit handler.

To troubleshoot, I created a minimal project with no additional middleware (bare minimum setup), and in that setup, the srand() function works without any issues.

However, in my main project where I need both lwIP and FreeRTOS, calling srand() causes an exit. The project was created following this guide:
How to Create a Project for STM32H7 with Ethernet and lwIP Stack.

I made one modification to the guide: instead of using the default OS wrapper, I selected CMSIS_V2.

Currently, I am only using the M7 core.

What I’ve Tried So Far

  • Minimal project without lwIP and FreeRTOS -> srand(12345) works fine.
  • Project with lwIP and FreeRTOS -> srand(12345) causes an exit.

I’ve attached an image showing the callstack where the issue occurs. I hope this helps in diagnosing the problem.

Here’s a link to my code: GitHub Repository

Does anyone have any ideas on what might be causing this issue? Could it be related to the use of CMSIS_V2, a conflict with FreeRTOS, or possibly a memory issue?

Thank you in advance for your help!

Best regards,
Oskar

Callstack.JPG

23 REPLIES 23

Yes I got the Hardfault with your latest software but without srand() call (I commented it). So the question is: are you sure srand() is what causing your original issue?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

I think the srand problem and the new hard fault are two separate issues. The srand issue was caused by the linker script. I feel like the hard fault is a software bug where the &hdr->sipaddr gets placed unaligned in the microcontroller's memory.

Should I mark this problem as solved and start a new thread for the hard fault issue?

My Nucleo should arrive tomorrow. Then I can dive deeper into this problem.

As they are a separate issue need to close this thread by Accepting as Solution the comment that guided you to the answer of the subject/question : "Issue with srand() causing exit in STM32H747 Project with FreeRTOS and lwIP"

and open a new thread for this new issue with a new description.

Thank you

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

I found the problem: I messed up the TEX level in the Memory Protection Unit settings.

I mistakenly set the TEX level for the second region instead of the first region.
I’ve attached the latest code for reference. This code runs without any faults on my device.