cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with creating event flag in ThreadX

mahirmahota
Associate III

When I call the tx_event_flags_create() function, the code returns an error at the following line:

 else if (event_control_block_size != (sizeof(TX_EVENT_FLAGS_GROUP)))
    {

        /* Event flags group pointer is invalid, return appropriate error code.  */
        status =  TX_GROUP_ERROR;
    }

I'm not sure why this would be a problem since I only have one TX_EVENT_FLAGS_GROUP defined in my program as far as I can see and the size of the struct passed in should match. Is there anything I could possibly be missing here?

7 REPLIES 7
mbarg.1
Lead

Add the code where you declare global

TX_EVENT_FLAGS_GROUP   event_control_block

 

add code where you compute 

event_control_block_size 

and code tx_event_flags_create() ... and i will show you where is the problem ! 

Or double check:

you need to have a global variable with the structure TX_EVENT_FLAGS_GROUP 

+ pass the address of this variable (not the variable) to tx_event_flags_create()

+ tx_event_flags_create() returns a success code, TX_SUCCESS if everithing is ok or an error code !

So the event flag variable is declared here at the top of my app_usbx_device.c:

TX_EVENT_FLAGS_GROUP EventFlag;

 And then inside MX_USBX_Device_Init, the flag is created and throws the error:

if (tx_event_flags_create(&EventFlag, "Event Flag" != TX_SUCCESS) {
    return TX_GROUP_ERROR
}

The event_control_block_size is computed in the tx_api.h file here:

#define tx_event_flags_create(g,n)    _txe_event_flags_create((g),(n),(sizeof(TX_EVENT_FLAGS_GROUP)))

 Both TX_EVENT_FLAGS_GROUP declarations seem to link to the same struct in tx_api.c hence why I was confused since the size should be the same here. Can you catch anything I might be overlooking?

But how do you compute your variable 

event_control_block_size 

??

That's the third argument passed into _txe_event_flags_create. Here's the function prototype:

UINT _txe_event_flags_create(TX_EVENT_FLAGS_GROUP *group_ptr, CHAR *name_ptr, UINT event_control_block_size);

 

But this variable is valid only inside that function, it is not global !

Use debugger and display in real time the value of this variable, eventually stepping through the code.

Yes, but the following check is also inside that function.

else if (event_control_block_size != (sizeof(TX_EVENT_FLAGS_GROUP))) 
{
    /* Event flags group pointer is invalid, return appropriate error code.  */
    status =  TX_GROUP_ERROR;
}

However, event_control_block_size is 36 while the sizeof(TX_EVENT_FLAGS_GROUP) is 40 even though they should be equal since the control block size is evaluated from the same expression if that makes sense.

I guess I understood the problem.

You have a problem with a ThreadX function

UINT  _txe_event_flags_create(TX_EVENT_FLAGS_GROUP *group_ptr, CHAR *name_ptr, UINT event_control_block_size)
{

TX_INTERRUPT_SAVE_AREA

UINT                        status;
ULONG                       i;
TX_EVENT_FLAGS_GROUP        *next_group;
#ifndef TX_TIMER_PROCESS_IN_ISR
TX_THREAD                   *thread_ptr;
#endif


    /* Default status to success.  */
    status =  TX_SUCCESS;

    /* Check for an invalid event flags group pointer.  */
    if (group_ptr == TX_NULL)
    {

        /* Event flags group pointer is invalid, return appropriate error code.  */
        status =  TX_GROUP_ERROR;
    }

    /* Now check for proper control block size.  */
    else if (event_control_block_size != (sizeof(TX_EVENT_FLAGS_GROUP)))
    {

        /* Event flags group pointer is invalid, return appropriate error code.  */
        status =  TX_GROUP_ERROR;
    }
    else
    {

        /* Disable interrupts.  */
        TX_DISABLE

  .......

where TX_EVENT_FLAGS_GROUP is defined as below

/* Define the event flags group structure utilized by the application.  */

typedef struct TX_EVENT_FLAGS_GROUP_STRUCT
{

    /* Define the event flags group ID used for error checking.  */
    ULONG               tx_event_flags_group_id;

    /* Define the event flags group's name.  */
    CHAR                *tx_event_flags_group_name;

    /* Define the actual current event flags in this group. A zero in a
       particular bit indicates the event flag is not set.  */
    ULONG               tx_event_flags_group_current;

    /* Define the reset search flag that is set when an ISR sets flags during
       the search of the suspended threads list.  */
    UINT                tx_event_flags_group_reset_search;

    /* Define the event flags group suspension list head along with a count of
       how many threads are suspended.  */
    struct TX_THREAD_STRUCT
                        *tx_event_flags_group_suspension_list;
    UINT                tx_event_flags_group_suspended_count;

    /* Define the created list next and previous pointers.  */
    struct TX_EVENT_FLAGS_GROUP_STRUCT
                        *tx_event_flags_group_created_next,
                        *tx_event_flags_group_created_previous;

    /* Define the delayed clearing event flags.  */
    ULONG               tx_event_flags_group_delayed_clear;

#ifdef TX_EVENT_FLAGS_ENABLE_PERFORMANCE_INFO

    /* Define the number of event flag sets.  */
    ULONG               tx_event_flags_group_performance_set_count;

    /* Define the number of event flag gets.  */
    ULONG               tx_event_flags_group__performance_get_count;

    /* Define the number of event flag suspensions.  */
    ULONG               tx_event_flags_group___performance_suspension_count;

    /* Define the number of event flag timeouts.  */
    ULONG               tx_event_flags_group____performance_timeout_count;
#endif

#ifndef TX_DISABLE_NOTIFY_CALLBACKS

    /* Define the application callback routine used to notify the application when
       an event flag is set.  */
    VOID                (*tx_event_flags_group_set_notify)(struct TX_EVENT_FLAGS_GROUP_STRUCT *group_ptr);
#endif

    /* Define the port extension in the event flags group control block. This
       is typically defined to whitespace in tx_port.h.  */
    TX_EVENT_FLAGS_GROUP_EXTENSION

} TX_EVENT_FLAGS_GROUP;

 Now it seems that in some functions sizeof(TX_EVENT_FLAGS_GROUP) evaluate to 40 and some time to 36.

This can arise:

  • if some code is compiled with TX_DISABLE_NOTIFY_CALLBACKS defined while in some other place is undefined
  • if TX_EVENT_FLAGS_GROUP_EXTENSION is defined with a uint32_t or other 4 bytes element.

Post the whole project

or try yourself to debug with Include browser, after re-indexing and rebuilding after cleaning all compiled, including static libraries.

mike

P.S.: do not forget to mark as solved, if my suggestions are correct.