2023-10-24 7:20 PM - last edited on 2024-07-08 7:22 AM by Amel NASRI
Hi,
I am having issues with threadX tx_byte_allocate throwing a hard fault exception.
This only happens after some time of byte allocate and release. There are still plenty of available bytes according to the pool. But somehow in _tx_byte_pool_search it encounters some problem.
I am not posting the entire source code here as that will be huge. Anyway, I am using STM32H753. I created a byte pool using DTCRAM (128K).
Linker snippet:
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
.ram_dtcmram :
{
*(.ram_dtcmram)
} >RAM
Code Snippet
#define RAM_DTCMRAM \
__attribute__((section(".ram_dtcmram")))
#define GENERIC_MEM_ALLOCATION (0x20000-0x1000)
static u8 m_genericMemBytePoolBuffer[GENERIC_MEM_ALLOCATION] RAM_DTCMRAM;
static TX_BYTE_POOL m_genericMemBytePool RAM_D3;
bool Hal_MemPool_Init(void)
{
if (tx_byte_pool_create(&m_genericMemBytePool, "Generic memory pool", m_genericMemBytePoolBuffer , GENERIC_MEM_ALLOCATION) != TX_SUCCESS){
return FALSE;
}
return TRUE;
}
This is the screenshot of the pool when the hard fault happens. byte pool available is still more than 50k
Below are the local variables during the fault. As you can see current pointer goes to 0x2492bc7e. That memory is not available for H753 and obviously will throw a hard fault error trying to access this memory.
Specifically on line below inside the do while(examine_blocks != ((UINT) 0)) loop
work_ptr = TX_UCHAR_POINTER_ADD(current_ptr, (sizeof(UCHAR *)));
free_ptr = TX_UCHAR_TO_ALIGN_TYPE_POINTER_CONVERT(work_ptr);
if ((*free_ptr) == TX_BYTE_BLOCK_FREE) //<-----------HARD FAULT
Now my question is why? Clearly, I have enough available bytes in the pool. You can also see below that the memory required is only 256 bytes. Even if the memory gets fragmented, I am pretty confident there is a block with 256 bytes free on it. Besides, ThreadX is supposed to merge those splits or fragments. Which is also stated in the pool above (tx_byte_pool_performance_merge_count)
Version of ThreadX is
Not that it matters I think, I made the pool m_genericMemBytePool the same RAM as the m_genericMemBytePoolBuffer to dtcmram. Same outcome.
Thanks,
Carlo
Solved! Go to Solution.
2023-10-26 5:11 PM
Issue reported to MSFT
2023-10-26 5:11 PM
Issue reported to MSFT
2024-12-20 1:33 AM
hello!
i have the exact same problem using a nucleo-g0b1re
tx_byte_allocate trow me an hardfault
digging n the code the hardfault appear at this line in the UCHAR *_tx_byte_pool_search(TX_BYTE_POOL *pool_ptr, ULONG memory_size)
if ((*free_ptr) == TX_BYTE_BLOCK_FREE) <---- hardfaukt here
the strange thing is that the same tx_byte_allocat function perfectly without another thread that i have recently added
i espect that if there is no room to allocate memory the tx_byte_allocate simply return different from TX_SUCCESS
(i'm using TX_WAIT_FOREVER so in fact i espect to wait)
but:
1) i sure have space in the byte pool
2) why an hardfault?
if i place the mouse on *free_ptr the value is : 0x20000026 <_impure_data+18>
did you find the problem?
i saw you close the ticket because you are porting a code from another OS but for me is totally a new code
best reguards