2021-07-01 05:09 AM
I'm registered for STM32Cube with Azure RTOS - Discovery workshops - Advanced hands-on workshop details. I do not have a Windows post, should I give up the workshop?
Best regards.
2021-07-01 05:39 AM
Hello,
the workshop is using STM32CubeIDE that runs on Linux.
Only limitation will be related to the usage of TraceX which is a Microsoft tool only running only on Windows.
But this limitation is will not prevent you to take advantage of the workshop content.
Even, I would not be surprised if this TraceX tools works find with wine...
Best regards
Jocelyn