cancel
Showing results for 
Search instead for 
Did you mean: 

Is there an example or manual for sending a UDP package with the Nucleo F429ZI?

MKlee
Associate

I have the Nucleo-144 Board with the STM32F429 Microprocessor. I'm really desperate.

Tanks for Help

1 REPLY 1
Imen.D
ST Employee

Hello,

I recommend you to have a look to the LwIP examples under STM32CubeF4 firmware package: STM32Cube_FW_F4_V1.21.0\Projects\STM32469I_EVAL\Applications\LwIP\

This can help you in your application and you may re-use sections available in the examples.

I suggest you to follow the following resources which can help you to go further in your application: 

  • UM1713 : “Developing applications on STM32Cube with LwIP TCP/IP stack�? .
  • AN3966 : “LwIP TCP/IP stack demonstration for STM32F4x7 microcontrollers�? 

With Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen