2023-04-18 7:19 AM
I am developing on the STM32U5 family and i need to use UCPD. As far as I know the UCPD middleware is no supported on this family, so I need to implement my functionality using the LL driver for the UCPD module. I am not experienced with usb power delivery. It would be nice to see and example of the ll_ucpd usage.
Solved! Go to Solution.
2023-04-20 5:26 AM - edited 2023-11-20 7:48 AM
Hi @MCseh.377
It looks like a link problem. Undefined symbols as USBPD_PE_Init, are expected to be present in the USBPD Core library.
Please check that you have such lib in the objects of your project : below picture is an example of USBPD MW lib in case of IAR Ewarm project.
Regards
2023-04-18 7:56 AM
Hi @MCseh.377
I confirm that STM32U5 embeds a UCPD peripheral for USB Power Delivery feature support. The STM32CubeU5 package contains USBPD Middleware (USB Power Delivery Stack + U5 Device) that is illustrated in some USBPD applications running on STM32U5 boards.
USBPD Middleware is provided in following directory in the STM32CubeU5 package : Middlewares\ST\STM32_USBPD_Library or here on Github.
Application example are provided for each board in Projects\<Board Name>\Applications\USBPD directory. For example you could find an example of a SNK application for STM32U5 Discovery board (B-U585I-IOT02A) here.
Regards
2023-04-20 4:12 AM - edited 2023-11-20 7:48 AM
Thank you @Guenael Cadier for your help,
I checked the example and I followed this tutorial to set up my usbpd sink device:
However after code generation i cannot build the project.
I am using STM32U575-Nucleo board, building it with the cubemx generated Makefile.
I get the following errors:
I don't find definitions for these functions, only declarations in the header files.
Can you help me where I messed up? :)
Thanks and best regards,
Mark
2023-04-20 5:26 AM - edited 2023-11-20 7:48 AM
Hi @MCseh.377
It looks like a link problem. Undefined symbols as USBPD_PE_Init, are expected to be present in the USBPD Core library.
Please check that you have such lib in the objects of your project : below picture is an example of USBPD MW lib in case of IAR Ewarm project.
Regards