cancel
Showing results for 
Search instead for 
Did you mean: 

internal temperature sensor stm32h743zit6

SITARAM
Associate III

I am using stm32h743zit6 ,but when i use below code in nucleo -H743zi2 and thermal camera.when i run below code in nucleo board then vref(vots) value coming 3.3 vots and temperature comming in 30 to 37 celcius but same code when i run in thermal camera vref (vots) value coming 3.3 vots but temperature very high(approximetly) 127 and moving above in celcius .so in thermal camera why same code gives temperature very high ????????????????????

CUBE MX INITILIZE

FIRST I TAKEN ADC3 AFTER THAT i taken temperature  sensor channel ,vrefint channel .

BELOW PARAMETERS

1.ADC_RESOLUTION_16B

2.ADC_CLOCK_ASYNC_DIV6

3. ADC_SAMPLETIME_387CYCLES_5;

SO WHAT CAN I DO GIVE ME SOLUTION !!!!!!!!!!!!!!!!!!!!!!!!!!

MAIN.C
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */
float vrefint_volts;
float temperature_celsius;
uint32_t vrefint = 0;

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
uint32_t adcValue;
float temperature,temperature_1;

float Read_Temperature(void)
{
  
HAL_ADCEx_Calibration_Start(&hadc3, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED);
    // Start ADC conversion
	  HAL_Delay(100);
    // Start ADC Conversion
    HAL_ADC_Start(&hadc3);

    // Poll for conversion completion
    if (HAL_ADC_PollForConversion(&hadc3, HAL_MAX_DELAY) == HAL_OK)
    {
        // Get ADC value
        adcValue = HAL_ADC_GetValue(&hadc3);
    }

    // Stop ADC conversion
    HAL_ADC_Stop(&hadc3);

		
		 // Read the calibration values
    uint16_t cal1 = *TEMPSENSOR_CAL1_ADDR;
    uint16_t cal2 = *TEMPSENSOR_CAL2_ADDR;
    uint16_t vrefint_cal = *VREFINT_CAL_ADDR;

    // Calculate the analog reference voltage (Vref+) in millivolts
   vrefint = __HAL_ADC_CALC_VREFANALOG_VOLTAGE(vrefint_cal, ADC_RESOLUTION_16B);

     vrefint_volts = vrefint / 1000.0f;  // Convert millivolts to volts

//    // Calculate temperature in degrees Celsius
   temperature_celsius = (float)__HAL_ADC_CALC_TEMPERATURE(vrefint, adcValue, ADC_RESOLUTION_16B);
   

    return temperature_celsius;
}
int main(void)
{
 
  HAL_Init();

  
  SystemClock_Config();

 
  MX_ADC3_Init();
 
  while (1)
  {
   
     temperature_1 = Read_Temperature();
		 HAL_Delay(1000);
   
  }
 
}
ADC.C
void MX_ADC3_Init(void)
{
  ADC_ChannelConfTypeDef sConfig = {0};

  /** Common config
  */
  hadc3.Instance = ADC3;
  hadc3.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV6;
  hadc3.Init.Resolution = ADC_RESOLUTION_16B;
  hadc3.Init.ScanConvMode = ADC_SCAN_DISABLE;
  hadc3.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
  hadc3.Init.LowPowerAutoWait = DISABLE;
  hadc3.Init.ContinuousConvMode = DISABLE;
  hadc3.Init.NbrOfConversion = 1;
  hadc3.Init.DiscontinuousConvMode = DISABLE;
  hadc3.Init.ExternalTrigConv = ADC_SOFTWARE_START;
  hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
  hadc3.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
  hadc3.Init.Overrun = ADC_OVR_DATA_PRESERVED;
  hadc3.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
  hadc3.Init.OversamplingMode = DISABLE;
  if (HAL_ADC_Init(&hadc3) != HAL_OK)
  {
    Error_Handler();
  }
  /** Configure Regular Channel
  */
  sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;
  sConfig.Rank = ADC_REGULAR_RANK_1;
  sConfig.SamplingTime = ADC_SAMPLETIME_387CYCLES_5;
  sConfig.SingleDiff = ADC_SINGLE_ENDED;
  sConfig.OffsetNumber = ADC_OFFSET_NONE;
  sConfig.Offset = 0;
  sConfig.OffsetSignedSaturation = DISABLE;
  if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }

}
ADC.H
#else /* ADC_VER_V5_90 || ADC_VER_V5_X */
#define TEMPSENSOR_CAL1_ADDR               ((uint16_t*) (0x1FF1E820UL)) /* Internal temperature sensor, address of parameter TS_CAL1: On STM32H7, temperature sensor ADC raw data acquired at temperature  30 DegC (tolerance: +-5 DegC), Vref+ = 3.3 V (tolerance: +-10 mV). */
#define TEMPSENSOR_CAL2_ADDR               ((uint16_t*) (0x1FF1E840UL)) /* Internal temperature sensor, address of parameter TS_CAL2: On STM32H7, temperature sensor ADC raw data acquired at temperature 110 DegC (tolerance: +-5 DegC), Vref+ = 3.3 V (tolerance: +-10 mV). */
#endif /* ADC_VER_V5_3 */

#define TEMPSENSOR_CAL1_TEMP               (30L)                        /* Internal temperature sensor, temperature at which temperature sensor has been calibrated in production for data into TEMPSENSOR_CAL1_ADDR (tolerance: +-5 DegC) (unit: DegC). */
#define TEMPSENSOR_CAL2_TEMP               (110L)                       /* Internal temperature sensor, temperature at which temperature sensor has been calibrated in production for data into TEMPSENSOR_CAL2_ADDR (tolerance: +-5 DegC) (unit: DegC). */
#define TEMPSENSOR_CAL_VREFANALOG          (3300UL)                     /* Analog voltage reference (Vref+) voltage with which temperature sensor has been calibrated in production (+-10 mV) (unit: mV). */

SYTEM CLOCK
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
  RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};

  /** Supply configuration update enable
  */
  HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
  /** Configure the main internal regulator output voltage
  */
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

  while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
  /** Macro to configure the PLL clock source
  */
  __HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSI);
  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
  RCC_OscInitStruct.PLL.PLLM = 4;
  RCC_OscInitStruct.PLL.PLLN = 50;
  RCC_OscInitStruct.PLL.PLLP = 2;
  RCC_OscInitStruct.PLL.PLLQ = 2;
  RCC_OscInitStruct.PLL.PLLR = 2;
  RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
  RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
  RCC_OscInitStruct.PLL.PLLFRACN = 0;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
                              |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
  RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
  RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
  {
    Error_Handler();
  }
  PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_ADC;
  PeriphClkInitStruct.PLL2.PLL2M = 4;
  PeriphClkInitStruct.PLL2.PLL2N = 9;
  PeriphClkInitStruct.PLL2.PLL2P = 1;
  PeriphClkInitStruct.PLL2.PLL2Q = 2;
  PeriphClkInitStruct.PLL2.PLL2R = 2;
  PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_3;
  PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOMEDIUM;
  PeriphClkInitStruct.PLL2.PLL2FRACN = 3072;
  PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLL2;
  if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
}
1 REPLY 1
SofLit
ST Employee

Why are you still duplicating the same thread?:

https://community.st.com/t5/moderation-archive/stm32h743zit6-internal-temperature-sensor-reading/td-p/714041

https://community.st.com/t5/stm32-mcus-embedded-software/stm32h743zit6-internal-temperature-sensor-reading/td-p/714067

https://community.st.com/t5/stm32-mcus-embedded-software/internal-temperature-sensor-stm32h743zit6/td-p/716065

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.