2018-09-17 11:36 PM
Hello Everyone
I'm trying to evaluate this microcontroller since some days. The goal is to use it into an embedded solution for data acquisition.
Is important to read microcontroller temperature and internal reference to improve precision.
I've successfully read analogs input into polling mode or interrupt mode (with or without DMA).
Unfortunately, in any case, I can't read Internal analogs (VrefInt and Temperature sensor).
Some tips for me.
Thanks in advance
Diego
2018-09-17 11:54 PM
From RM0316:
Note: To convert one of the internal analog channels, the corresponding analog sources must first
be enabled by programming bits VREFEN, TSEN or VBATEN in the ADCx_CCR registers.
I don't Cube.
JW
2018-09-18 12:31 AM
I think the Cube/HAL library should program those bits as long as you select the corresponding ADC channel.
In ainterrupt mode, the callback (HAL_ADC_ConvCpltCallback) should be triggered once per channel, in the order of their rank. Then you only have to keep track of which channel is triggering it and read the value with the HAL_ADC_GetValue (hadc) function.
Hope this hleps
Julien
2018-09-18 01:38 AM
Hi waclawek.jan
I checked these bits are already setted by CubeMX generated code in "stm32f3xx_hal_adc_ex.c" file.
Not working anyway
/* If the requested internal measurement path has already been enabled, */
/* bypass the configuration processing. */
if (( (sConfig->Channel == ADC_CHANNEL_TEMPSENSOR) &&
(HAL_IS_BIT_CLR(tmpADC_Common->CCR, ADC_CCR_TSEN)) ) ||
( (sConfig->Channel == ADC_CHANNEL_VBAT) &&
(HAL_IS_BIT_CLR(tmpADC_Common->CCR, ADC_CCR_VBATEN)) ) ||
( (sConfig->Channel == ADC_CHANNEL_VREFINT) &&
(HAL_IS_BIT_CLR(tmpADC_Common->CCR, ADC_CCR_VREFEN)))
)
{
/* Configuration of common ADC parameters (continuation) */
/* Set handle of the other ADC sharing the same common register */
ADC_COMMON_ADC_OTHER(hadc, &tmphadcSharingSameCommonRegister);
/* Software is allowed to change common parameters only when all ADCs */
/* of the common group are disabled. */
if ((ADC_IS_ENABLE(hadc) == RESET) &&
( (tmphadcSharingSameCommonRegister.Instance == NULL) ||
(ADC_IS_ENABLE(&tmphadcSharingSameCommonRegister) == RESET) ) )
{
/* If Channel_16 is selected, enable Temp. sensor measurement path */
/* Note: Temp. sensor internal channels available on ADC1 only */
if ((sConfig->Channel == ADC_CHANNEL_TEMPSENSOR) && (hadc->Instance == ADC1))
{
SET_BIT(tmpADC_Common->CCR, ADC_CCR_TSEN);
/* Delay for temperature sensor stabilization time */
/* Compute number of CPU cycles to wait for */
wait_loop_index = (ADC_TEMPSENSOR_DELAY_US * (SystemCoreClock / 1000000U));
while(wait_loop_index != 0U)
{
wait_loop_index--;
}
}
/* If Channel_17 is selected, enable VBAT measurement path */
/* Note: VBAT internal channels available on ADC1 only */
else if ((sConfig->Channel == ADC_CHANNEL_VBAT) && (hadc->Instance == ADC1))
{
SET_BIT(tmpADC_Common->CCR, ADC_CCR_VBATEN);
}
/* If Channel_18 is selected, enable VREFINT measurement path */
/* Note: VrefInt internal channels available on all ADCs, but only */
/* one ADC is allowed to be connected to VrefInt at the same */
/* time. */
else if (sConfig->Channel == ADC_CHANNEL_VREFINT)
{
SET_BIT(tmpADC_Common->CCR, ADC_CCR_VREFEN);
}
}
Thanks
Diego
2018-09-18 01:51 AM
Hi julien1.536826307249236E12
Yes i did but not working :(
Thanks
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc){
if (hadc->Instance == ADC1){
//end of conversion
if (__HAL_ADC_GET_FLAG(&hadc1, ADC_FLAG_EOC)){
/* Get ADC1 converted data */
ADC1ConvertedValue[ADCIndex] = HAL_ADC_GetValue(&hadc1);
ADCIndex++;
}
//end of sequence, restarting
if (__HAL_ADC_GET_FLAG(&hadc1, ADC_FLAG_EOS)){
ADCIndex = 0;
}
}
}