cancel
Showing results for 
Search instead for 
Did you mean: 

Instructions on how to load flash memory code: 0x90000000

NguyenAnhHieu_
Associate II

Hi everyone, I am using STM32H745BIT6 and programming using W25Q128. I am trying to upload the code but always get an error at the last step.

STMicroelectronics ST-LINK GDB server. Version 7.10.0

Copyright (c) 2025, STMicroelectronics. All rights reserved.

Starting server with the following options:

Persistent Mode            : Disabled

Logging Level      : 1

Listen Port Number: 61234

Status Refresh Delay       : 15s

Verbose Mode                : Disabled

SWD Debug                 : Enabled

InitWhile                 : Enabled

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

-------------------------------------------------------------------

STM32CubeProgrammer v2.19.0

-------------------------------------------------------------------

Log output file:   C:\Users\hieua\AppData\Local\Temp\STM32CubeProgrammer_a22168.log

ST-Link Server is running on port : 7184

ST-LINK SN : 130019000D0000383036544E

ST-LINK FW : V2J46S7

Board       : --

Voltage     : 3.10V

SWD freq    : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID   : 0x450

Revision ID : Rev V

Device name: STM32H7xx

Flash size : 2 MBytes

Device type : MCU

Device CPU : Cortex-M7/M4

BL Version : 0x91

Opening and parsing file: ST-LINK_GDB_server_a22168.srec

Memory Programming...

File         : ST-LINK_GDB_server_a22168.srec

Size         : 4.98 KB

Address       : 0x08100000

Erasing memory corresponding to sector 0:

Erasing internal memory sector 8

Download in Progress:

File download complete

Time elapsed during download operation: 00:00:03.382

Verifying...

Download verified successfully

-------------------------------------------------------------------

STM32CubeProgrammer v2.19.0

-------------------------------------------------------------------

Log output file:   C:\Users\hieua\AppData\Local\Temp\STM32CubeProgrammer_a22168.log

ST-Link Server is running on port : 7184

ST-LINK SN : 130019000D0000383036544E

ST-LINK FW : V2J46S7

Board       : --

Voltage     : 3.10V

SWD freq    : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID   : 0x450

Revision ID : Rev V

Device name: STM32H7xx

Flash size : 2 MBytes

Device type : MCU

Device CPU : Cortex-M7/M4

BL Version : 0x91

Opening and parsing file: ST-LINK_GDB_server_a22168.srec

Memory Programming...

File         : ST-LINK_GDB_server_a22168.srec

Size         : 185.59 KB

Address       : 0x08000000

Erasing memory corresponding to sector 0:

Erasing internal memory sectors [0 1]

Erasing memory corresponding to sector 0:

Erasing external memory sector 0

Error: failed to erase memory

Error: failed to erase memory

Encountered Error when opening E:\STM32\IDE\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.100.202412061334\tools\bin\STM32_Programmer_CLI.exe

Error in STM32CubeProgrammer

Shutting down...

Exit.

I have referenced the build here: https://controllerstech.com/w25q-flash-series-part-10-qspi-ext-loader-in-h750/ and https://www.youtube.com/watch?v=XqCq0xtQmbI&list=PLnMKNibPkDnHIrq5BICcFhLsmJFI_ytvE&index=7

3 REPLIES 3
jumman_JHINGA
Senior III

@NguyenAnhHieu_  You selected wrong stldr file. try to get correct external loader from https://github.com/cturvey/stm32extldr/blob/main  GIT.

Thanks, but unfortunately when designing the hardware I chose a pin configuration that was completely different from the pre-made files. So I had to find a way to create the .stldr file

NguyenAnhHieu__0-1744174166700.png

 

KDJEM.1
ST Employee

Hello @NguyenAnhHieu_ ;

 

->So I had to find a way to create the .stldr file

I recommend you to look at How to create an external QSPI loader MOOC and get inspired to create the own .stldr file. This MOOC explains how to create an external QSPI loader for STM32CubeProgrammer.

 

I hope this help you.

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.