cancel
Showing results for 
Search instead for 
Did you mean: 

In AN4488 is says that STM32F413 MCU uses pins PB5/PB13 if you want to program the MCU via CAN interface. Is it possbile to remap the CAN pheripherals to other pins and still be able to use the embedded bootloader or is it thigtly coupled to pins PB5/PB13

ØKris.1
Associate
1 ACCEPTED SOLUTION

Accepted Solutions
prain
Senior III

No, not possible for ST Bootloader. But feasible for a custom Bootloader.

View solution in original post

4 REPLIES 4

> Is it possbile to remap the CAN pheripherals to other pins and still be able to use the embedded bootloader

No.

JW

TDK
Guru

You can remap those pins for your application, but the bootloader will only listen on PB5/PB13.

If you feel a post has answered your question, please click "Accept as Solution".
prain
Senior III

No, not possible for ST Bootloader. But feasible for a custom Bootloader.

ØKris.1
Associate

Thx for the replies :)