cancel
Showing results for 
Search instead for 
Did you mean: 

implemented TCP/IP ,UDP,HTTP PROTOCAL

Asing.3
Associate II

hello all

currently i am working on Free RTOS (STM32L152RETX microcontroller ) . in stmcubemx no any one feature to implement the any protocal like TCP/ip etc

is there any possiblities to implement this protocal by using STM32L152RETx microcontroller

if yes then how

3 REPLIES 3
Ozone
Lead II

The L15x MCUs have no ethernet MAC, so no.

There will be no direct support by ST or ST tools.

But third-party vendors offer boards or companion chips implementing ethernet/TCP-IP, and translate it to one of the usual serial protocols.

I remember Microchip had one of those, can't remember the type name - I never used it.

That adds quite a bit to the BOM, though.

Asing.3
Associate II

okk sir

Asing.3
Associate II

i will try