2020-08-28 5:03 AM
I want to wakeup from standby-mode in less than 20msec.
I want to wake up from standby-mode in less than 20 seconds using Periodic auto-wakeup, but I can't wake up below 22 msec.
Could you tell me if there is any good way?
The following HAL driver is used.
HAL_RTCEx_SetWakeUpTimer( & hrtc,1,RTC_WAKEUPCLOCK_RTCCLK_DIV2 );
And the MCU is STM32L433.
Thanks in advance!
2020-08-29 7:45 PM
Hello YTaka.1
First make sure your LSE/RTC is well calibrated, you can use the 1Hz RTC_output to be sure of that.
In RM0394 section 36.3.6 Periodic auto-wakeup, it say "When the periodic wakeup interrupt is enabled by setting the WUTIE bit in the RTC_CR register, it can exit the device from low-power modes." So I guess give HAL_RTCEx_SetWakeUpTimer_IT a try.
I suggest also to test, without entering the standby mode, the time between two wakeup event by the RTC, just to better understand how your system behave.
Good luck,
Regards,
Hajji.