2018-05-02 2:01 PM
Posted on May 02, 2018 at 23:01
When using the STM32L100C-Disco Board i use the command,
HAL_PWR_EnterSTANDBYMode()
but when I measure the current on I_DDpins using a multimeter on the uA setting (using a Fluke 87), I read a value of ~282uA, which is higher than the spec sheet which says ~3uA. Any ideas why? Are there additional commands that need to be called prior to entering standby mode? Could it be the type of multimeter I am using? I disable the wakeup pins and I made all the pins Analogue inputs before entering standbymode.
Thanks.
2018-05-04 11:47 AM
Looks like a current leakage.
I found interesting note for STM32L15x (not exactly the one you use but also from L1 series):
Page 7:
'The slilicon limitation present on STM32L15xxB PB7 pin may affect current consumption measurement. When PB7 is configured in analog mode and no PVD level is selected, an internal pull-up is activated on PB7 pin. This may induce current flow through external components such as resistors or diode on the STM32L1-DISCOVERY board. To measure only the MCU current consumption, two solutions are possible:
•Disconnect the LD3 diode connected to PB7 internal pull-up
•Configure PB7 as an input and connect PB7 pin to GND to minimize current consumption.
'
I do not want to say that this is the root cause....
2018-05-10 1:06 AM
I tried what you suggested, but it did not work. Any other suggestions?