cancel
Showing results for 
Search instead for 
Did you mean: 

I've created a project for stm32H745 (dual core) and add the threadX support from software package, but I see it only for the CM4, not the CM7 (and I have also free-rtos selected which is enforced for both). Is it correct?

EDallaVia
Associate II
 
3 REPLIES 3
EDallaVia
Associate II

also, does the cubemx put together both free-rtos and threadx or if I choose threadx it superseed the free-rtos?

0693W00000WL5zYQAT.pngmany thanks

EDallaVia
Associate II

My apologies, the checks are indeed active but if you click over CM4 the rtos setting is desabled

Haithem Rahmani
ST Employee

Hi @EDallaVia​ ,

Indeed STM32CubeMX does not allow using FreeRTOS & ThreadX in the same project, you'll need to select one.

regards

Haithem.