2022-02-15 01:50 PM
2022-02-25 07:11 AM
Hello,
Please check this Github repository, there are some FreeRTOS examples (ioc not available) for NUCLEO-U575ZI-Q that might be helpful.
@David Littell , We still don't know when will FreeRTOS be supported in CubeMX for U5. We will inform you as soon as we have any news.
Sara.
2022-02-16 12:33 AM
Hello @Community member ,
Thanks for your feedback,
For U5 family, there is only AzureRTOS available. FreeRTOS is not supported.
If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly
Thanks for your contribution and do not hesitate to raise any issue/ feedback.
Sara.
2022-02-16 02:42 AM
Thanks for response. mbedOS is supported?
2022-02-16 03:05 AM
Hello @Community member ,
What I meant with my first reply is that FreeRTOS middleware is not available for U5 in CubeMX but it is possible to work with it.
mbedOS is also not available in CubeMX but yes U5 is supported.
Both OS are available on Github.
I hope this helps
Sara.
2022-02-16 08:21 AM
When will FreeRTOS for the U5 be properly supported in CubeMX?
2022-02-25 07:11 AM
Hello,
Please check this Github repository, there are some FreeRTOS examples (ioc not available) for NUCLEO-U575ZI-Q that might be helpful.
@David Littell , We still don't know when will FreeRTOS be supported in CubeMX for U5. We will inform you as soon as we have any news.
Sara.
2022-06-10 01:04 PM
Hello @Sara BEN HADJ YAHYA
Is there any updated ETA on FreeRTOS support for B-U585I-IOT02A. Using the FreeRTOS repo for NUCLEO-575ZI-Q is quite lacking given there are so many additional chips (wifi, bt) on the discovery board. it has been very time consuming to do things that were much easier in earlier boards. It's a bit disconcerting to see support for FreeRTOS being jettisoned so quickly. Please keep in mind using AzureRTOS is not an option for everyone. Any update on this would be deeply appreciated.
2022-06-10 02:03 PM
Adding FreeRTOS takes literally few minutes...
http://www.radekdostal.com/content/freertos-610-minimal-example
2022-06-10 02:20 PM
We have no problem running FreeRTOS on the board, it's the support for the additional chips on this board that we are asking for (Wifi+BT). The ST moderators clearly understand this based on their original responses.
2022-07-14 12:53 PM
ST Cube support for B-U585I-IOT02A with FreeRTOS is all packaged in this June 2022 release from ST: