cancel
Showing results for 
Search instead for 
Did you mean: 

[STM32H743XGH6] Flash memory

NiM
Associate III

I believe the STM32H743XGH6 has 1 MB of internal flash memory. However, using STM32CubeProgrammer, I was able to write and read data to the reserved area at 0x8180 0000. Is it okay to use this area?

The built-in Flash Memory areas of the STM32H743XGH6 are recognized as
0x8100 0000-0x817F FFFF and 0x8000 0000-0x0801 FFFF.

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

This zone of Flash is physically available but not tested in production so its usage is not guaranteed: its usage is  NOT recommended.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
mƎALLEm
ST Employee

Hello,

This zone of Flash is physically available but not tested in production so its usage is not guaranteed: its usage is  NOT recommended.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.