2025-08-22 2:01 PM
Hello,
I have implemented a sdcard socket on my board based on the STM32F411,
I use SDIO & fatfs r0.15c p2,
The SDIO DMA NVIC configuration is :
/* DMA2_Stream3_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream3_IRQn, 6, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream3_IRQn);
/* DMA2_Stream6_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream6_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream6_IRQn);DMA
/* SDIO DMA Init */
/* SDIO_RX Init */
hdma_sdio_rx.Instance = DMA2_Stream3;
hdma_sdio_rx.Init.Channel = DMA_CHANNEL_4;
hdma_sdio_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_sdio_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_sdio_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_sdio_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
hdma_sdio_rx.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
hdma_sdio_rx.Init.Mode = DMA_PFCTRL;
hdma_sdio_rx.Init.Priority = DMA_PRIORITY_VERY_HIGH;
hdma_sdio_rx.Init.FIFOMode = DMA_FIFOMODE_ENABLE;
hdma_sdio_rx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_sdio_rx.Init.MemBurst = DMA_MBURST_INC4;
hdma_sdio_rx.Init.PeriphBurst = DMA_PBURST_INC4;
if (HAL_DMA_Init(&hdma_sdio_rx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hsd,hdmarx,hdma_sdio_rx);
/* SDIO_TX Init */
hdma_sdio_tx.Instance = DMA2_Stream6;
hdma_sdio_tx.Init.Channel = DMA_CHANNEL_4;
hdma_sdio_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_sdio_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_sdio_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_sdio_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
hdma_sdio_tx.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
hdma_sdio_tx.Init.Mode = DMA_PFCTRL;
hdma_sdio_tx.Init.Priority = DMA_PRIORITY_VERY_HIGH;
hdma_sdio_tx.Init.FIFOMode = DMA_FIFOMODE_ENABLE;
hdma_sdio_tx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_sdio_tx.Init.MemBurst = DMA_MBURST_INC4;
hdma_sdio_tx.Init.PeriphBurst = DMA_PBURST_INC4;
if (HAL_DMA_Init(&hdma_sdio_tx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hsd,hdmatx,hdma_sdio_tx);My PLL configuration
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 25;
RCC_OscInitStruct.PLL.PLLN = 384;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 8;SDIO
hsd.Instance = SDIO;
hsd.Init.ClockEdge = SDIO_CLOCK_EDGE_RISING;
hsd.Init.ClockBypass = SDIO_CLOCK_BYPASS_DISABLE;
hsd.Init.ClockPowerSave = SDIO_CLOCK_POWER_SAVE_DISABLE;
hsd.Init.BusWide = SDIO_BUS_WIDE_1B;
hsd.Init.HardwareFlowControl = SDIO_HARDWARE_FLOW_CONTROL_DISABLE;
hsd.Init.ClockDiv = 1;
/* USER CODE BEGIN SDIO_Init 2 */
//hsd.Init.BusWide = SDIO_BUS_WIDE_1B;
if (HAL_SD_Init(&hsd) != HAL_OK){
log_error("MX_SDIO_SD_Init: error HAL_SD_Init code:%d",hsd.ErrorCode);
}
if (HAL_SD_ConfigWideBusOperation(&hsd, SDIO_BUS_WIDE_4B) != HAL_OK){
log_error("MX_SDIO_SD_Init: HAL_SD_ConfigWideBusOperation error code:%d",hsd.ErrorCode);
}
With some SD Card that are not HC, but V10 I have f_write issue with fatfs return code 1
const char string[512];
sprintf(string,"HELLO HERE");
unsigned int pt;
FILINFO fno;
/* Open or create a log file and ready to append */
printf("mount:%d\n",f_mount(&fs, "", 1));
printf("open: %d\n", f_open(&file, "log.txt", FA_WRITE | FA_OPEN_ALWAYS ));
printf("stat: %d\n", f_stat("log3.txt", &fno));
printf("write: %d wr: %d\n", f_write(&file, string, 512, &pt), pt);
printf("flush: %d\n", f_sync(&file));
printf("close: %d\n", f_close(&file)); /* close performs sync before close */if (clst == 0xFFFFFFFF) ABORT(fs, FR_DISK_ERR);
fp->clust = clst; /* Update current cluster */
2025-08-22 2:31 PM
Hi,
what format the cards have ? same ?
Did you enable exfat in fatfs ?
2025-08-22 3:51 PM
The SDCard is formatted using the same format type between the 2 SD Card => Fat32
Exfat is not enable...
Vincent