How to reading wakeup flag?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-29 3:45 AM
I want to know which Wakeup pin or Reset pin wakes up the microprocessor that enters standby mode. I have 2 wakeup pins.
I am monitoring SR1 and SR2 variables with Live expression in Debug mode, but when I wake up from standby mode, the value of the variables does not change.
Is there a method other than the code block below?
I am grateful in advance.
/* USER CODE BEGIN 2 */
CheckWakeupPins();
/* USER CODE END 2 */
/* USER CODE BEGIN 4 */
void CheckWakeupPins(void) {
// Ensure the PWR clock is enabled
__HAL_RCC_PWR_CLK_ENABLE();
// Read the wakeup pin status from PWR_SR1
uint32_t wakeup_status = __HAL_PWR_GET_FLAG(PWR_FLAG_WU);
// Check individual wakeup pins - adjust mask as per your device's definitions
SR1 = (wakeup_status & PWR_FLAG_WUF1) ? 1 : 0;
SR2 = (wakeup_status & PWR_FLAG_WUF2) ? 1 : 0;
HAL_Delay(3000);
// Clear the wakeup flags after processing to avoid retriggering
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
}
/* USER CODE END 4 */
- Labels:
-
STM32Cube MCU Packages
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-29 6:46 AM
Hello,
method you are using is correct, but in masking wakeup flag don´t use PWR_FLAG_WUF1 but PWR_SR1_WUF1 and instead of PWR_FLAG_WUF2 use PWR_SR1_WUF2 and it should work fine.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-29 7:52 AM
void EnterStandbyMode(void)
{
// Enable Power Peripheral
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN2);
// Clear PWR Wake-up Flag
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
// Enable WKUP pin
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN2);
// Enter STANDBY Mode
HAL_PWR_EnterSTANDBYMode();
}
void CheckWakeupReason(void)
{
if(__HAL_RCC_GET_FLAG(RCC_FLAG_PINRST)) {
// [Wakeup Reason] Hardware Reset Pin
}
if(__HAL_RCC_GET_FLAG(RCC_FLAG_SFTRST)) {
// [Wakeup Reason] Software Reset
}
if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB)) {
// [Wakeup Reason] Standby Mode
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-01 6:48 AM
You can see the coding in the attached image.
When both WKUP pins are woken up, only the LED named GPIO_PIN_8 lights up.
So WUF2 is never HIGH.
GPIO_PIN_8 when woken up with pin 1,
GPIO_PIN_7 should work when woken up with pin 2, but GPIO_PIN_8 works even when I wake it up with pin 2.