2022-04-28 5:25 AM
Hello,
I am configuring KSZ8863 3 port switch over I2C. And the slave address Read/Write address is oxBF/0xBE respectively. In the HAL reference manual it says the address should be shifted left before calling the interface. It's confusing, if I am shifting it (0xBE <<1), the address becomes 0x7C. Or the HAL_I2C transmit will handle the address even if shifted?
Also, should I send the address as 0xBF while using HAL_I2C_Receive ?
Below are the HAL functions used in my code.
HAL_I2C_Master_Transmit(&hi2c1, KSZ8863_WRITE_ADDRESS, buf, 2, HAL_MAX_DELAY);
HAL_I2C_Master_Receive(&hi2c1,KSZ8863_READ_ADDRESS, Data, 1, HAL_MAX_DELAY);
Thanks
2022-04-28 5:51 AM
This is confusing because sometimes, a 7-bit address is published and sometimes an already shifted 8-bit address. Since 0xBE hat the MSB set, it must be already shifted. This conforms to the data sheet:
Two fixed 8-bit device addresses are used to address KSZ8863MLL/FLL/RLL in I2C Slave mode: one for read operation and the other for write operation. The addresses are as follows:
• 1011_1111 <read>
• 1011_1110 <write>
Pass 0xBE to the HAL functions. HAL will handle the LSB for read/write correctly.
One may also use HAL_I2C_IsDeviceReady to search the I2C bus for responding target devices.
hth
KnarfB
2022-04-28 8:40 PM
@KnarfB Thank you very much for the clarity.