Skip to main content
HXiao.1
Associate II
February 10, 2021
Question

How to config UART in STM32F446?

  • February 10, 2021
  • 2 replies
  • 1925 views

I'm using STM32F446, I found one issue.

  1. In STM32F4xx_hal_uart.c, it stated that.

 ==============================================================================

            ##### How to use this driver #####

 ==============================================================================

 [..]

  The UART HAL driver can be used as follows, pay attention to the last line about UART pins, it's stated that RX as alternate function input.

  (#) Declare a UART_HandleTypeDef handle structure (eg. UART_HandleTypeDef huart).

  (#) Initialize the UART low level resources by implementing the HAL_UART_MspInit() API:

    (##) Enable the USARTx interface clock.

    (##) UART pins configuration:

      (+++) Enable the clock for the UART GPIOs.

      (+++) Configure these UART pins (TX as alternate function pull-up, RX as alternate function Input).

  1. When I generate code by CubeMX, the generated code in function HAL_UART_MspInit, GPIO_PIN_3 is RX, and GPIO_PIN_2 is TX, but both of them are configured the same. It's different from the description in STM32F4xx_hal_uart.c. I tested, and found that the CubeMX generated code works. If I configure GPIO_PIN_3 as GPIO_MODE_INPUT, UART does not work, is the comment in STM32F4xx_hal_uart.c wrong?

    GPIO_InitStruct.Pin = GPIO_PIN_2 | GPIO_PIN_3;

    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

    GPIO_InitStruct.Pull = GPIO_PULLUP;

    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

    GPIO_InitStruct.Alternate = GPIO_AF7_USART2;

    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
February 10, 2021

> is the comment in STM32F4xx_hal_uart.c wrong?

Yes.

There's no "alternate function input"

Except in the old 'F1 family, if you set a pin to AF in GPIO_MODER (and assign some AF in respective GPIO_AFR), the module to which this pin is assigned controls the direction of that pin. UARTs set Rx pin to Input, Tx to Output, as soon as you enable the receiver/transmitter/UART in UART_CR1.

JW

ST Technical Moderator
February 12, 2021

Hello @HXiao.1​ and welcome to the STM32 Community,

I escalated the wrong comment to the development team for correction in the coming releases.

Thanks for your contribution.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks