2020-01-21 04:18 PM
In the demo for Keyboard or Mouse, its one or the other,
how can you run a Keyboard and a Mouse ?
2020-01-27 10:01 PM
mention part number ,
2020-01-27 11:57 PM
it is a H743 board
the device "cap touch" is limping along on FS Host,
luckily the touch chip responds with the data I need, so one finger is running
but when I plug in the Keyboard HS host the touch dies but the keyboards works
then unplug and nothing works, guess I should trap that and deinit/reinit
Still unable to send a control packet to the touch chip, not sure how to. couldn't find an example.
Could you point me to the description of "report type " or a usage example of this: