cancel
Showing results for 
Search instead for 
Did you mean: 

how import git project?

kliurka
Visitor

how to import this project: https://github.com/lucysrausch/stm32-turbotronik ?

I test importing with (EGit - integration for Eclipse 6.7.0) extension from Eclipse market, but not success (Build icon is not active) same if importing from local directory.

Thanks in advance for help

8 REPLIES 8
Pavel A.
Evangelist III

Click on green button <Code> , select "download ZIP".

 

SofLit
ST Employee

Hello @kliurka and welcome to the community,

See this article: https://community.st.com/t5/stm32-mcus/downloading-stm32cube-packages-from-github-correctly/ta-p/725288

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

@Pavel A. wrote:

 select "download ZIP".


According to the knowledgebase article linked by @SofLit,  that won't work - because it won't fetch submodules

I make File>New>Project(clean project), then File>Import>ArchiveFile and same - Build icon not active..

SofLit
ST Employee

@kliurka wrote:

I test importing with (EGit - integration for Eclipse 6.7.0) extension from Eclipse market,


Are you using STM32CubeIDE?

I recommend to import the package with git and refer to the link I shared before.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

@SofLit wrote:

 

Are you using STM32CubeIDE?

I recommend to import the package with git and refer to the link I shared before


STM32CubeIDE

Version: 1.16.1

Build: 22882_20240916_0822 (UTC)

 


@SofLit wrote:

See this article: https://community.st.com/t5/stm32-mcus/downloading-stm32cube-packages-from-github-correctly/ta-p/725288




same problem - not active Build

 


@kliurka wrote:



same problem - not active Build


Not sure what do you mean by not active build.

Cloning the github link you shared and the link you shared using this git command and succeeded to get the repository:

git clone --recursive https://github.com/lucysrausch/stm32-turbotronik

 Now I don't see any STM32CubeIDE project in it.

So need to contact the project developer on how to build the project.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

That repo does not have submodules.

And it is not an Eclipse project at all. Just a makefile project.