2024-10-10 07:41 AM
how to import this project: https://github.com/lucysrausch/stm32-turbotronik ?
I test importing with (EGit - integration for Eclipse 6.7.0) extension from Eclipse market, but not success (Build icon is not active) same if importing from local directory.
Thanks in advance for help
2024-10-10 08:38 AM
Click on green button <Code> , select "download ZIP".
2024-10-10 09:12 AM
Hello @kliurka and welcome to the community,
See this article: https://community.st.com/t5/stm32-mcus/downloading-stm32cube-packages-from-github-correctly/ta-p/725288
2024-10-10 09:15 AM
2024-10-10 09:24 AM
I make File>New>Project(clean project), then File>Import>ArchiveFile and same - Build icon not active..
2024-10-10 09:27 AM
@kliurka wrote:
I test importing with (EGit - integration for Eclipse 6.7.0) extension from Eclipse market,
Are you using STM32CubeIDE?
I recommend to import the package with git and refer to the link I shared before.
2024-10-10 10:05 AM
@SofLit wrote:
Are you using STM32CubeIDE?
I recommend to import the package with git and refer to the link I shared before
STM32CubeIDE
Version: 1.16.1
Build: 22882_20240916_0822 (UTC)
@SofLit wrote:See this article: https://community.st.com/t5/stm32-mcus/downloading-stm32cube-packages-from-github-correctly/ta-p/725288
same problem - not active Build
2024-10-10 10:15 AM
@kliurka wrote:
same problem - not active Build
Not sure what do you mean by not active build.
Cloning the github link you shared and the link you shared using this git command and succeeded to get the repository:
git clone --recursive https://github.com/lucysrausch/stm32-turbotronik
Now I don't see any STM32CubeIDE project in it.
So need to contact the project developer on how to build the project.
2024-10-10 10:25 AM - edited 2024-10-10 10:27 AM
That repo does not have submodules.
And it is not an Eclipse project at all. Just a makefile project.