2019-02-06 02:55 AM
I have STM32F469I Discovery Evaluation kit. Target is to implement the acoustic Echo cancellation. But not able to find osxAcousticEC library middleware. Please provide the same or suggest suitable solution.
2019-02-06 04:53 AM
Hello,
The osxAcousticEC software package has been replaced by FP-AUD-SMARTMIC1.
So, you can use FP-AUD-SMARTMIC1, this firmware runs on the STM32 and includes drivers and middleware for digital MEMS microphones and audio output management.
It includes middleware for Echo Cancellation.
For mode details, please have a look on the Quick start guide.
Kind Regards,
Imen
2019-02-06 05:04 AM
Thanks for the reply.
I have STM32F469 DISCOVERY board with me & I want to run the example project provided along with library. And this new library required NUCLEO board & Microphone board to run the example project.
So I request here to provide the old library, which can supports to DISCOVERY board example projects, similar to attached application note.