2022-08-29 7:01 AM
After testing P-NUCLEO-USB002 kit with it's embedded demonstration example I try to use different example from en.STSW-STUSB010 examples- it seems like non of them support UART interface (CLI) as in P-NUCLEO-USB002 embedded demonstration example. my questions are: 1. How can I get the P-NUCLEO-USB002 embedded demonstration example? 2. Is there a way to enable UART interface (CLI) in en.STSW-STUSB010 examples? Thanks, Maor
2022-10-18 5:12 AM
I unfortunately have the same Problem after I flashed one of the Projects from the en.STSW-STUSB010 Library.
2022-10-19 10:10 AM