2022-05-23 10:09 AM
Actually, my aim is to get data from a digiducer sensor with STM32F0 via USB port and can't understand how.
2022-05-23 10:40 AM
The sensor connects via USB?
Does you STM32F0 provide for a USB HOST?
It it does assume you'll need to write a suitable CLASS DRIVER
2022-05-24 3:04 AM
yes the sensor connects only with USB.
and when i was searching for the right STM32 MCU to get data from this connector, i found the STM32F0 that has inside a USB device as shown in the figure below.
is there any piece of help about this CLASS driver to base on or a helpful document to assume this USB communication?
2022-05-24 4:08 AM
You know what you're doing?
In the headline you write about "microphone USB", in the description you mention a USB sensor.
USB device means that you can connect it to a USB host (for example a computer), not that you can connect other USB devices, such as your sensor.
2022-05-24 4:41 AM
Thank you LCE for the explanation.
actually, according to my understanding, I thought that Microphone USB and My sensor ( in my case, a digiducer for vibration that has a USB connector) give the same data, that's why i mentioned both of them.
I'm a student and I'm working on an academic project in which i have to read data from this sensor with STM32F0. via USB and don't know how.
if you can guide me, I will be so thankful.
2022-05-24 5:33 AM
> i have to read data from this sensor with STM32F0. via USB
You cannot.
As I said: STM32F0 is a USB device only, as far as I understand the STM32F0 website.
You need an STM32 with USB host / on the go capabilities, which the STM32F0 does not have.
Maybe the assignment is a little bit different, like:
connect a sensor (not via USB) to an STM32F0, then send sensor data from STM32F0 via USB to PC.
?
2022-05-24 6:50 AM
@amlok.1 "I'm a student"
Then you should be going to your teacher/supervisor for assistance: they know you, and the task you've been assigned, and the resources available to you - we know none of that.
"i have to read data from this sensor with STM32F0. via USB"
As the others have said, you cannot.
A USB connection always consists of a Host, and a Device (ignoring Hubs for now).
Your sensor is a USB Device - therefore you will need a USB Host to connect to it.
As it says in the diagram you posted, the STM32F0 is also a USB Device - it cannot connect to another USB Device.
This is fundamental to the way USB works - it is not anything specific to the STM32
2022-05-24 8:06 AM
ok, now I understand what you said.
in my case, the sensor( digiducer) can only be connected by USB. I need to get data from it and stock it in an MCU ( if you can suggest me a host that can work among the STM MCUs ).
2022-05-24 8:10 AM
Thank you @Andrew Neil for the clarification.
Do you know an MCU that can get this data for my sensor via USB because this is the only way it can connect?
2022-05-24 8:31 AM
I don't have an extensive list, perhaps you can do a parametric search on the part via the website, but the F2, F4, F7 and H7 all have models which support USB HOST, and USB DEVICE operational modes.