cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I am using STM32F769I-DISCO.In SDK I am Using SDJPEG example. In the code File open function is working fine but file closing is not working. Can anyone sort out this issue?

DM.14
Associate
1 REPLY 1
FBL
ST Employee

Hello @DM.14​,

Do you refer to this example? If yes, could you make sure that HAL_JPEG_GetInfo is retrieving the image parameters properly?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.