HAL_HCD_IRQHandler only happens once
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-23 9:41 PM
Hi everyone.
We have run a project on discovery f746 board consist of FREE RTOS , emwin and fat fs sd card library,that it works fine.
Now we want to add USB OTG Host in FS mode to our project.
We tried to append configurations of MSC_Standalone sample to our project and unfortunately it didn't work.
We debugged the code and it seems &sharpifdef USE_USB_FS is not defined in our project.
Also after reset the board while the USB flash is connected to board interrupt of USB ( HAL_HCD_IRQHandler(&hhcd); ) happens one time and It does not happen anymore.
What should we do?
Any suggestions.
Thanks in advance!
#rtos #core #stm32-interrupt #host-driver #usb- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-25 10:28 PM
Hi everyone.
We have these four functions at the beginning of the thread.
Menu_Init();
/* Init Host Library */ USBH_Init(&hUSBHost, USBH_UserProcess, 0); /* Add Supported Class */ USBH_RegisterClass(&hUSBHost, USBH_MSC_CLASS); /* Start Host Process */ USBH_Start(&hUSBHost);After these ,we created a window from emwin library.
In this window when press one of the buttons , these two functions run.
/* USB Host Background task */
USBH_Process(&hUSBHost);/* MSC Menu Process */
Appli_state = APPLICATION_READY; MSC_MenuProcess();All of these functions were copied from
MSC_Standalone sample.
But as i said,
interrupt of USB ( HAL_HCD_IRQHandler(&hhcd); ) happens one time.
Please give us some suggestions to find out and resolve the problem.
Thanks a lot.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-07-09 1:13 AM
Hi all,
I also ran into a similar problem while using the RTOS together with custom USB Host class driver. I noticed that the enumeration of the device could no be performed because the USBH_Core state machine never reaches the HOST_DEV_ATTACHED state, In fact the
HAL_HCD_IRQHandler(&hhcd) is not called anymore. I suspect that at some point the interruptions are disabled but i can&39t figure out where.
#rtos
#stm32%20interrupt
#
#host%20driver
#