cancel
Showing results for 
Search instead for 
Did you mean: 

Force STM32Cube MCU Package update in project.

Carlos Diaz R.
Associate III

Hi,

I had been working with a project using a STM32F411RE device, with the STM32F4 package version 1.24.0. I installed the version 1.24.1 and would like to update the project, but when i open the Cube project it doesn't ask me for the update.

Is there any way to force the update manually?

1 REPLY 1
KnarfB
Principal III

In the STM32CubeMX project manager tab, if you uncheck the "Use latest available version" you should be able to choose the correct version from the drop-down list.